This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

msp430f5229两个SPI不能同时用?

Other Parts Discussed in Thread: CC1120

以下是我对时钟配置和两个SPI的配置初始化代码

//调试时钟配置
void halInitMCU(void)
{
  WDTCTL = WDTPW + WDTHOLD;                 // Stop watchdog timer
 
 
  //
  P5SEL |= BIT2+BIT3;                       // Port select XT2
  UCSCTL6 &= ~XT2OFF;                       // Enable XT2
  UCSCTL3 |= SELREF_2;                      // FLLref = REFO
                                            // Since LFXT1 is not used,
                                            // sourcing FLL with LFXT1 can cause
                                            // XT1OFFG flag to set
  UCSCTL4 |= SELA_2;                        // //ACLK=REFO,SMCLK=DCO,MCLK=DCO
}


//初始化与CC1120连接的spi
void CC1120_SpiInit(void)
{
  volatile unsigned int i;

  WDTCTL = WDTPW+WDTHOLD;                   // Stop watchdog timer

  P1DIR |= BIT7;                            // Set P1.7 for CSN
  P2DIR |= BIT3;                            // Set P2.3 for slave reset
  P3SEL |= BIT3+BIT4;                       // P3.3,4 option select
  P2SEL |= BIT7;                            // P2.7 CLK
 
  UCA0CTL1 |= UCSWRST;                      // **Put state machine in reset**
  UCA0CTL0 |= UCMST+UCSYNC+UCCKPL+UCMSB;    // 4-pin, 8-bit SPI master
                                            //Clock polarity high, MSB
  UCA0CTL1 |= UCSSEL_3;                     // SMCLK
  UCA0BR0 = 0x02;                           // /2
  UCA0BR1 = 0;                              //
  UCA0MCTL = 0;                             // No modulation
  UCA0CTL1 &= ~UCSWRST;                     // **Initialize USCI state machine**
 
  P1OUT &= ~0x80;                           // p1.7 CSN low
 
  P2OUT &= ~0x08;                           // p2.3 Now with SPI signals initialized,
  P2OUT |= 0x08;                            // reset slave
 
                                         //The ISR for SPI RX Date/Tx Data
  for(i=50;i>0;i--);                        // Wait for slave to initialize

//  __bis_SR_register(LPM0_bits + GIE);       // CPU off, enable interrupts
}
//初始化与Flsah连接的spi
void Init_CC1120_SpiFlash()
{
  P2DIR |= BIT4;                            //CS_N ouput
  P3SEL |= BIT0+BIT1;                      // P3.0,1,2 option select
  P3SEL |= BIT2;                           // P3.2 clk
 
  UCB0CTL1 |= UCSWRST;                    // **Put state machine in reset**
  UCB0CTL0 |= UCMST+UCSYNC+UCCKPL+UCMSB+UCMODE0;  // 4-pin, 8-bit SPI slave,
                                            // Clock polarity high, MSB
  UCB0CTL1 |= UCSSEL_2;                     // SMCLK
//  UCB0BR0 = 0x00;                           // /2
//  UCB0BR1 = 0;                              //

  UCB0CTL1 &= ~UCSWRST;                     // **Initialize USCI state machine**
}