Other Parts Discussed in Thread: DP83640, LMK03000, CDCM9102
请教各位专家:
我准备把83640用在分布终端上,让各终端与中心站进行高精度的时间同步。 根据AN-1730,主从设备都需要25MNz的本地参考时钟,我目前用的晶振精度不高,只能达到ms级,中心站和终端侧需要什么样的时钟精度?需要多高的同步频率才能保持5ns以内的同步误差?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
谢谢您的专业答复。
那么如果我要在多个从设备间保证5ns内的误差,主从设备上都必须有前述精度的时钟配合吗?
AN1730里面第5段( 第7页)提到:
Finally, since the frequency of the master clock is delivered through the network, the stability of the local
oscillator is not a significant source of error when Synchronous Ethernet mode is enabled. The stability of
a slave node is directly dependent upon the stability of its corresponding PTP connected master node.
是否可以认为从设备上时钟精度要求不高,ms级晶振即可?
我看文档里面的测试例是用的TI 的LMK03000,但是看DASHEET这块芯片有7路时钟输出,而且要7刀一片,感觉很浪费的样子,不知有没有成本更低的方案?
CDCM9102只要2.25刀一片,可以满足要求吗?
我的总体需求是,我用以太网连接多个分布式终端和一个核心端,怎么才能让多个分布式设备上实现严格同步的时钟输出,误差最好控制在1ns以内,要用什么芯片方案实现呢?
哪位大神知道,请联系我,解我燃眉之急,感谢!