Part Number: TCA9517
I2C总线有最小电阻限制 一般为1.5K。
采用TCA9517缓冲器的话,A侧采用1.5K上拉电阻的,B测是否也可以采用1.5K上拉电阻。
问题点:TCA9517内部A和B是否是连通的?如果内部连通的话总线上拉为0.75K。 如果两侧单独电路的话就是各自测1.5K上拉,总线不会上拉并联为0.75K。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
首先I2C是open drain架构,所以两边都需要上拉。EN高电平时,SDAA=SDAB, SCLA=SCLB,导通的。
其次Rmin的最小值由Vol决定的,阻值再小的话低压就拉不下来了。
Rmin=(Vcc-Vol)/Iol.
手册上采用的上拉阻值为典型值10Kohm,您可以A,B两边通道都上拉10K就可以了。