This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BT.656转SDI问题

Other Parts Discussed in Thread: LMH0030, CLC020, CLC021, LMH0340, LMH0341, LMH0302, LMH0384

需求背景:

我有一台BT.656接口输出的热成像机芯,希望把他转成SDI接口。机芯的接口是D0~D7和CK,Y-Cb-Cr的4-2-2协议,640×480 25FPS(50i),电平是LVCOMS2.5V,使用温度-40-70度,同时探索有没有可能兼容BT.1120(16bit接口)(不重要),请问用什么方案可以实现?

我的考虑:

我在视频的硬件开发上没什么经验,在逐步学习中,初步思路是考虑用一个serializer+cable driver就可以。查了TI的器件,发现LMH0030、CLC020、CLC021理论上都支持SDTV 27MHz的接口转SDI,SDI的输出不需要配独立的cable driver,并口端输入电平也是OK的,所以我本来是希望外面搞个单片机来配置寄存器就好了,但唯一的遗憾是上述器件使用温度范围都达不到-40,这是个比较尴尬的事情。

我的问题如下,烦请帮助解答:

1 如果我直接用上述器件(不考虑温度问题)的话,8bit接口和器件的10bit接口怎么兼容,多出的2位需要怎么处理?

2 LMH0030貌似可以实现BT656和BT1120接口的兼容,那么接口在电路上需要如何处理才能实现兼容?

3 还有没有其他的解决方案可以搞定这个事儿,能够满足功能和温度的要求;

多谢。