请教一下,DS90UB935和DS90UB936是否能支持到1920*1280@50帧率的视频流?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,1920*1280*50*(1+15%)=141Mhz左右,而936在10bit data下的PCLK范围为20~100Mhz。12bit LF mode下为10~50Mhz,12bit HF mode下为15Mhz~75Mhz。
所以不能支持1920*1280@50帧率的视频流。
和936一样输出MIPI CSI数据类型的这类ADAs serdes器件吗?ADAs系列产品PCLK的汇总如下,可以看到最大100Mhz。
IVIxx系列的92x和94x在dual link应用下PCLK能支持到210Mhz,但应该是不满足您的应用要求的。