您好,我想使用ONET1101L芯片驱动激光二极管,在查看datasheet的过程中,看到输入端DIN+和DIN-分别是正向输入端和反向输入端
我想了解,
1、这个输入信号是一对差分信号吗?单端信号可以触发吗?如果可以,应该怎么连接这两个管脚?
2、DIN+和DIN-的电平情况,对芯片管脚MOD+和MOD-的影响是什么,对驱动激光器发光的影响是什么?
如果可以的话请提供一份设计说明。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
赵慧敏 您好,
ONET1101L主要用于高速数据传输。
DIN是差分输入模拟信号,可以更好的抑制高速信号的干扰,不建议使用单端输入信号。
DIN+, DIN–电压输入范围为供电电压范围。
DIN+, DIN–间的压差(VIN)在数据手册第4页“RECOMMENDED OPERATING CONDITIONS”中定义。
数据手册第2页“Figure 1”中显示了芯片的内部框图,DIN输入通过内部调制电路在MOD脚输出驱动电流。
www.ti.com/.../onet1101l.pdf