Other Parts Discussed in Thread: DP83640
自己参照demo板做的板子,网口连到电脑没有反应,怀疑是DP83640有问题,不知道怎么判断Dp83640正常工作,它正常工作GPIO口的电压应该是高电平还是低电平,忘各位大侠指教,万分感谢!还有谁有关于DP83640以及网口的正确接法的电路给小弟传一份啊!谢谢了
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我想问下,就是对以太网芯片进行读写,必须要将以太网电口和“电脑”连接才行吗?
Hi WeiCao,
MDIO读写PHY芯片可以单独进行,不必有以太网电缆连接对端。
Best Regards,
Shawn Han
你好!我想问下,在我使用光口的时候为什么上电后还需手动复位一次才行?而使用电口却不需要,这是为什么啊?谢谢…………!
1, 读取寄存器 PCSR, address 0x16,bit 6 FX_EN 状态, 1 = Enables FX operation, 0 = Disables FX operation. 看上电后DP83640是否已经进入FX模式。
2, 如果没有进入FX模式,请修改FX_EN=1,然后软复位Write PHYCR2[9], SOFT_RESET。
建议通过MCD,MDIO读一下DP93640的BMCR,BMSR,ANAR,ANLPAR, 看看PHY的 状态,硬件连接正确,PHY不需要配置,即可正常网络通讯。另外LED_SPEED灯亮,不能说明什么问题,因为这个灯是内部上拉,默认就是亮的。