1、iso3080芯片为422模式输出,是否可以A与Y短接,B与Z短接,用做485方式输出?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
不知你的问题解决了吗? 不论是半双工还是全双工,driver端输出都不对,发送端D的高电平最低不能低于2V,低电平最高不能超过0.8V,这个没问题吧?
有没有换块新的ISO3080试试?
半双工的话就是发送和接收不能同时进行,所以像你说的将DE和RE同时使能高低电平是没问题的。
全双工的话,就是发送和接收可以同时进行,就像ISO3080的架构一样,这样的话,DE为高,RE为低,AB是driver的输出端,D为输入,而YZ是receiver输入端,R为输出。