由于中秋、国庆节假期,帖子审批以及工程师回复将会有所延迟,敬请谅解.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1042: ISO1042

Part Number: ISO1042

Dear Ti Expert,

I would like to ask about ISO1042 IC applications. I have more than two devices using ISO1042.

Can I supply multiple ISO1042's VCC2 using one power supply?

I can't find information about the power supply application of VCC2 of ISO1042

You can provide more information on the power usage method of the CANBus side.

Please refer to my reference schematics.