This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMQ66430-2EVM: 5V 升压 5--30V (宽电压隔离输出)

Part Number: LMQ66430-2EVM
Other Parts Discussed in Thread: LMQ66430

我在TI 的官网买了一块  LMQ66430-2EVM demo板  回来测试,此demo板默认输出3.3V,测试的时候,将demo板电源输入口接可以测电流的设备,不接负载,实际测试下来 当输入电压13.5V 的时候,输出3.3V,此时电流0.704uA,如下图所示:

因为我后面的需求是输出5V,不是3.3V,要求此芯片待机IQ 极低,然后我就改了FB 上下电阻,RFBT 改成49.9K ,RFBB改成12.4K,输出变成了5V,同样的测试方法,电流变成了40uA左右,和3.3V 输出0.7uA 有很大的差异,不知道这是为什么呢?

LMQ66430 规格书写的 具有1.5uA IQ ,不会改成5V 输出就差异这么大吧?

有大神帮忙看看吗?怎么直接在此demo板直接修改元器件,改成5V 输出,电流也是1uA 左右呢?

谢谢