您好
请问TXS0104E-Q1是否具备VCC 隔离特性?
如果不具备那么VCCA/B其中一路电源掉电后,会有哪些失效?硬件设计要做哪些改进?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
不具备VCC 隔离特性。
TXS0104E-Q1 是电压电平转换芯片,VCCA和VCCB都要接供电电源。VCCA 电压范围是 1.65V 至 3.6V,A端口I/O参考VCCA电压;VCCB 电压范围是 2.3V 至 5.5V,B端口I/O参考VCCB电压, 同时需要VCCA ≤ VCCB。在工作过程中,需确保VCCA≤ VCCB;通电上电期间,VCCA≥ VCCB不会损坏设备,因此哪个电源都可以先启动。
对掉电一端的I/O输入信号是没有问题的,因为其I/O内部没有正偏二极管,见下面FAQ说明:
但是当只有VCCA通电时,会存在一定的风险,这是因为当VCCA上的电压超过VCCB上的电压时,内部保护二极管会变得正向偏置。当这种情况发生时,大量电流流过VCCA并流入二极管,从而增加功耗并可能损坏设备。因此,当为VCCA和VCCB使用单独的电源时,必须特别注意VCCA和VCCB是否在同一电压节点下工作。系统设计师必须确保电源公差不会导致VCCA和VCCB之间的电位差大到足以使内部保护二极管偏置。具体见下面手册的1.1章节:
https://www.ti.com/lit/an/scea060/scea060.pdf
如果需要所有输出都被置 于高阻抗状态,则需要将输出使能端 (OE) 输入为低电平,其 OE 管脚输入电路由 VCCA 供电。
下面帖子中工程师 ShreyasRao的一个测试结果可能对您有帮助,即 As we have tested this device, the IOs go to hi-Z and disconnects the pullups during one of the power supply is turned off.