Dear Ti
请问SN74LVC1G08-Q1 是否支持 down translation(也就是IC1.8V供电时,输入为3.3V )
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Ti
请问SN74LVC1G08-Q1 是否支持 down translation(也就是IC1.8V供电时,输入为3.3V )
谢谢!
您好,
SN74LVC1G08-Q1可以输入的电压范围可以到5.5V,因此在1.8V供电时,您可以输入3.3V的信号,但是需要看SN74LVC1G08-Q1在1.8V供电时是否可以正确识别输入的高低电平,如下截图识别范围:

是的,
当输入信号大于VCC电压时,主要考虑的是低电平,因为低电平更不容易满足规格。1.8V供电时,低电平电压要小于0.35VCC,即0.63V,而3.3V的信号低电平输出规格一般最大可能是0.3VCC,即0.3*3.3=0.99V,这就不能被SN74LVC1G08-Q1正确识别为低电平了。