This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV1T34: 压摆率

Part Number: SN74LV1T34
Other Parts Discussed in Thread: SN74LXC1T14, SN74LXC1T45, SN74LVC1T45

各位专家好:

在高频信号传输中,用到该器件,该期间未给出压摆率是多少,在2.5V方波信号到5V方波信号的转换过程中,20MHz以上的信号失真较为严重,能否给出相关参数或者更高压摆率电平转换芯片的推荐。

  • 您好,

    看datasheet 给出的开关特性,在5V供电时,支持最大到50MHZ的频率。在您的应用中,输出电容CL大概是多少?如果驱动的负载有容性或输出走线较长,CL较大,那么将影SN74LV1T34可以支持的信号的最大频率

  • 感谢回复,我主要用来对20MHz到50MHz的方波信号进行电平转换与整形,后续接的是栅极驱动IC,供电5V,对方波的质量要求较高,如果不适合的话有没有更好的应用推荐。

  • 看波形是RC充放电波形,应该就是CL太大的缘故,您可以具体测试下下面几款新品,驱动电流比 SN74LV1T34大一些,不知道实际应用波形质量是否满足您的设计要求?

    SN74LXC1T14

    SN74LXC1T45

    SN74LVC1T45