This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AXC4T774: 1.1V的SVID总线与3.3V的FPGA Pin间的电平转换方案咨询

Part Number: SN74AXC4T774

您好:

我们在评估电平转换方案,需要将1.1V的SVID总线与3.3V的FPGA的GPIO连接。SVID总线通信频率20MHz

SVID总线上有一个50Ω的电阻,下拉到0.2V附近需要一个下拉电流约为20mA的电平转换芯片。但是SN74AXC4T774芯片手册中显示单个Pin只有3mA的能力

想要问下是否可以将多个Pin并联使用,来增强下拉能力?也就是将下图的DIR1~4连在一起作为一个方向Pin,A1~A4连在一起,B1~B4连在一起,4路当作1路转换芯片来使用。是否可以这样应用?如果不可以的话,是否有低电压大驱动能力的芯片推荐?