This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AMC1200:紧急:针对不同的电流范围使用多个分流器

Guru**** 2925130 points

Other Parts Discussed in Thread: AMC1200

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/1131715/amc1200-urgent-using-multiple-shunts-for-different-current-ranges

器件型号:AMC1200

您好,  

我将 AMC1200用于以下配置的电流测量仪表。

如您所见,我正在使用多个串联分流器,其中它们之间的点连接到一个能够处理高达15A 电流的端子块。

例如,如果选择了10Ampere 范围(最大10Ampere),则电流将仅流经30m Ω 电阻器,产生300mV 的满量程

如果选择了5Ampere 范围、则用户将在第二个30m Ω 上插入电流、以便电流通过60m Ω、从而产生相同的满量程300mV  

我认为误差在1%到2%之间是可以的、但在发送光绘文件进行大规模生产之前、我需要快速查看原理图、因为我们无法制作原型。

非常感谢

BR

AMR Wael