This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LMV761:输入失调电压规格

Guru**** 1142300 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/986298/lmv761-input-offset-voltage-specification

器件型号:LMV761

您好!

数据表显示 Vos=0.2mV 典型值。 @ Ta=25°C 且 Vos=1mV 最大值 @ Ta=-40...+125°C

这意味着+/-0.2mV 和+/-1mV 的失调电压、还是+0.2mV/-0mV 和+1mV/-0mV?

此致、Oliver