请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM358-N 在数据表中、短路电流典型值为40mA。
如果电源电压为9V 且 Vo 与 GND 短路、则 LM358-N 上的总功率为360mW。
在数据表第4页上、DSBGA 绝对最大功耗典型值为435mW。
在9Vin、Vo 短路条件下、LM358-N 是否能够在没有额外保护电路的情况下承受?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.