请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:LAUNCLXL2-TMS5.7012万 主题中讨论的其它部件:TMS570LS1224
我正在尝试将CCS V11连接到Launchpad和BQ7.5614万EVM
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我正在尝试将CCS V11连接到Launchpad和BQ7.5614万EVM
您好,Sanon:
1.将LAUNCXL2连接到PC的USB端口
2.启动CCS视图-->目标配置
3.在Target Config (目标配置)窗口中,双击NewtargetCnfiguration.CCXML (您可以更改名称)

4.在NewTarget配置窗口中,选择xds110 USB调试器和TMS570LS1224,然后保存配置:

5.返回目标配置窗口,选择NewtargetConfiguration.CCXML,然后单击鼠标右键
6.启动选定的配置
7.在“调试”窗口中,将JTAG连接到目标。