主题中讨论的其他器件:LAUNCHXL2-570LC43
您好!
我希望 您在这段困难的19岁大的时期内保持健康。
我已经下载了一个从 QJ Wang 构建的关于电路板 LAUNCHXL2-570LC43的项目
当我尝试 将代码加载到主板时 ,我收到了以下消息:
CortexR5:加载程序:程序的一个或多个部分落在一个不可写的存储器区域中。 这些区域实际上不会写入目标。 检查链接器配置和/或存储器映射。
CortexR5:文件加载程序:验证失败:地址0xF0407FF0处的值不匹配请验证目标存储器和存储器映射。
CortexR5:GEL:文件:C:\Users\PC_1742_admin\Desktop\Hercules_Ethernet_Bootloader_deleted\build-LAUNCHXL2-TMS570LC43x-tftpboot\Debug\build-LAUNCHXL2-TMS570LC43x-tftpboot.out:发生数据验证错误、文件加载失败。
当我关闭 DE 验证时,会显示如下消息:
CortexR5:加载程序:程序的一个或多个部分落在一个不可写的存储器区域中。 这些区域实际上不会写入目标。 检查链接器配置和/或存储器映射。
我在 main.c 中更改了 GJ Wang 代码,如下所示;
/******************************************************************************************************** * * main.c : The main file for ethernet bootloader. * Author : QJ Wang. qjwang@ti.com * Date : 4-25-2021 */ /* Copyright (C) 2013-2020 Texas Instruments Incorporated - http://www.ti.com/ * * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /*--------------------------------------------------------------------------------------------------------------------- * Revision History *--------------------------------------------------------------------------------------------------------------------- * Version Date Author Description *--------------------------------------------------------------------------------------------------------------------- * 00.10.00 25/04/2021 QJ Wang 1. Initial Version ***********************************************************************************************************/ /* USER CODE BEGIN (0) */ /* USER CODE END */ /* Include Files */ #include "HL_sys_common.h" /* USER CODE BEGIN (1) */ #include "HL_system.h" #include "HL_gio.h" #include "HL_sci.h" #include "lwiplib.h" #include "bl_tftp.h" #include "bl_config.h" #include "uartstdio.h" #include "ustdlib.h" #include "HL_esm.h" /* USER CODE END */ /** @fn void main(void) * @brief Application main function * @note This function is empty by default. * * This function is called after startup. * The user can use this function to implement the application. */ /* USER CODE BEGIN (2) */ #define ENABLE_UPDATE_CHECK #define FORCED_UPDATE_PIN 4 //***************************************************************************** // // This holds the current address that is being written to during a download // command. //union //***************************************************************************** uint32_t g_ulTransferAddress; uint32_t g_pulUpdateSuccess[8] = {0x5A5A5A5A, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0}; uint32_t g_ulUpdateStatusAddr = APP_STATUS_ADDRESS; uint32_t g_ulUpdateBufferSize = 32; /*32 bytes */ void IntMasterIRQEnable (void); void sciDisplayText(sciBASE_t *sci, uint8_t *text,uint32_t length); uint32_t CheckGPIOForceUpdate(void); #if 1 extern unsigned int apiLoadStart; extern unsigned int apiLoadSize; extern unsigned int apiRunStart; extern unsigned int constLoadStart; extern unsigned int constLoadSize; extern unsigned int constRunStart; #endif /* USER CODE END */ uint8_t emacAddress[6] = {0x7C, 0xE6, 0xD3, 0x69, 0x8E, 0xD7}; //***************************************************************************** // // Display an lwIP type IP Address. // //***************************************************************************** void DisplayIPAddress(uint32_t ui32Addr) { char pcBuf[16]; // // Convert the IP Address into a string. // #if defined(_TMS570LC43x_) usprintf(pcBuf, "%d.%d.%d.%d", (ui32Addr >> 24) & 0xff, (ui32Addr >> 16) & 0xff, (ui32Addr >> 8) & 0xff, (ui32Addr >> 0) & 0xff); #endif #if defined(_RM57Lx_) usprintf(pcBuf, "%d.%d.%d.%d", ui32Addr & 0xff, (ui32Addr >> 8) & 0xff, (ui32Addr >> 16) & 0xff, (ui32Addr >> 24) & 0xff); #endif // // Display the string. // UARTprintf(pcBuf); } /* This example works for HDK*/ void main(void) { /* USER CODE BEGIN (3) */ unsigned int ipAddr; g_pulUpdateSuccess[1]= APP_START_ADDRESS; g_pulUpdateSuccess[3] = 0x20002021; /*version number, 02.00, in 2021*/ esmREG->SR1[0] = 0xFFFFFFFF; esmREG->SR1[1] = 0xFFFFFFFF; esmREG->SR1[2] = 0xFFFFFFFF; esmREG->SR4[0] = 0xFFFFFFFF; esmREG->EKR = 0x0A; esmREG->EKR = 0x00; /* Copy the flash APIs to SRAM*/ memcpy(&apiRunStart, &apiLoadStart, (uint32)&apiLoadSize); gioInit(); sciInit(); gioSetDirection(gioPORTB, 0xC0); sciSetBaudrate(UART, UART_BAUDRATE); /* Enable the interrupt generation in CPSR register */ _enable_IRQ(); UARTprintf("Ethernet lwIP Bootloader \n\r"); uint8 ip_addr[4] = { 192, 168, 0, 2}; uint8 netmask[4] = { 255, 255, 255, 0 }; uint8 gateway[4] = { 192, 168, 0, 3}; bool isProcessDone = false; bool isPressed = false; if(((*(uint32_t *) APP_STATUS_ADDRESS) == 0x5A5A5A5A)) { UARTprintf("ITS ENTER HERE................................."); g_ulTransferAddress = (uint32_t)APP_START_ADDRESS; // ((void (*)(void))g_ulTransferAddress)(); } while (!isProcessDone) { if(!gioGetBit(gioPORTB, 4)) { isPressed = true; gioToggleBit(gioPORTB, 6); } if (!ipAddr) { ipAddr = lwIPInit(0, emacAddress, *((uint32_t *)ip_addr), *((uint32_t *)netmask), *((uint32_t *)gateway), IPADDR_USE_STATIC); gioSetBit(gioPORTB, 7, 0); } else { gioSetBit(gioPORTB, 7, 1); } UARTprintf("HDK IP Address: "); DisplayIPAddress (ipAddr); UARTprintf(" \n\r "); if(isPressed) { break; // isProcessDone = true; // isPressed = false; // gioSetBit(gioPORTB, 6, 0); // gioSetBit(gioPORTB, 7, 0); } } TFTPQSInit(); // If the isPressed ( TO BUTTON GPIOB_4 EXIT FROM WHILE LOOP AND COMES HERE. ) UARTprintf("DONE "); } void sciDisplayText(sciBASE_t *sci, uint8_t *text,uint32_t length) { while(length--) { while ((sci->FLR & 0x4) == 4); sciSendByte(sci,*text++); }; } void IntMasterIRQEnable(void) { _enable_IRQ(); return; } void IntMasterIRQDisable(void) { _disable_IRQ(); return; } unsigned int IntMasterStatusGet(void) { return (0xC0 & _get_CPSR()); } /* ** Interrupt Handler for Core 0 Receive interrupt */ volatile int countEMACCore0RxIsr = 0; #pragma INTERRUPT(EMACCore0RxIsr, IRQ) void EMACCore0RxIsr(void) { countEMACCore0RxIsr++; lwIPRxIntHandler(0); } /* ** Interrupt Handler for Core 0 Transmit interrupt */ volatile int countEMACCore0TxIsr = 0; #pragma INTERRUPT(EMACCore0TxIsr, IRQ) void EMACCore0TxIsr(void) { countEMACCore0TxIsr++; lwIPTxIntHandler(0); } //***************************************************************************** // // Checks a GPIO for a forced update. // // This function checks the state of a GPIO to determine if a update is being // requested. // // \return Returns a non-zero value if an update is being requested and zero // otherwise. // //***************************************************************************** #ifdef ENABLE_UPDATE_CHECK uint32_t CheckGPIOForceUpdate(void) { /** bring GIO module out of reset */ gioREG->GCR0 = 1; gioREG->ENACLR = 0xFF; gioREG->LVLCLR = 0xFF; // Set the pin as input gioPORTA->DIR &= ~(1 << FORCED_UPDATE_PIN); // Enable the pull up/down. gioPORTA->PULDIS &= ~(1 << FORCED_UPDATE_PIN); // Enable the weak pull up. gioPORTA->PSL |= 1 << FORCED_UPDATE_PIN; // Check the pin to see if an update is being requested. if ((gioPORTA->DIN & (0x1 << FORCED_UPDATE_PIN) ) == 0) { // Remember that this was a forced update. return(1); //force to update } // No update is being requested so return 0. return(0); } #endif /* USER CODE END */