This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSPM0G3107:SysConfig 在 TIMG 比较模式下不生成 edgeDetectMode

Guru**** 2535750 points
Other Parts Discussed in Thread: SYSCONFIG

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1241092/mspm0g3107-sysconfig-does-not-generate-edgedetectmode-in-timg-compare-mode

器件型号:MSPM0G3107
主题中讨论的其他器件:SysConfig

尊敬的 Champs:

使用 MSPM0 SDK v1.0.1.3和 SysConfig 1.16.2时、如果将计时器配置为在比较模式下从事件触发器进行计数、则不会为结构 gTIMER_....CompareConfig 生成 edgeDetectMode。 这意味着 CCCTRL_01寄存器中的 ACOND 位未设置、因此计时器无法正常工作。 此结构成员应设置为 DL_TIMER_COMPARE_EDGE_DETECTION_MODE_RISING。

如果您确认这是 SysConfig 或 SDK 中的错误、您可以提交查询以修复该错误吗?


此致、
François μ A。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    这是 SYSCFG 文件:

    /**
     * These arguments were used when this file was generated. They will be automatically applied on subsequent loads
     * via the GUI or CLI. Run CLI with '--help' for additional information on how to override these arguments.
     * @cliArgs --device "MSPM0G350X" --package "VQFN-32(RHB)" --part "Default" --product "mspm0_sdk@1.00.01.03"
     * @versions {"tool":"1.16.2+3028"}
     */
    
    /**
     * Import the modules used in this configuration.
     */
    const Board    = scripting.addModule("/ti/driverlib/Board");
    const COMPARE  = scripting.addModule("/ti/driverlib/COMPARE", {}, false);
    const COMPARE1 = COMPARE.addInstance();
    const GPIO     = scripting.addModule("/ti/driverlib/GPIO", {}, false);
    const GPIO1    = GPIO.addInstance();
    const GPIO2    = GPIO.addInstance();
    const GPIO3    = GPIO.addInstance();
    const GPIO4    = GPIO.addInstance();
    const SYSCTL   = scripting.addModule("/ti/driverlib/SYSCTL");
    const SYSTICK  = scripting.addModule("/ti/driverlib/SYSTICK");
    const WWDT     = scripting.addModule("/ti/driverlib/WWDT", {}, false);
    const WWDT1    = WWDT.addInstance();
    
    /**
     * Write custom configuration values to the imported modules.
     */
    const gate7  = system.clockTree["MFCLKGATE"];
    gate7.enable = true;
    
    const oscillator2           = system.clockTree["SYSOSC"];
    oscillator2.enableSYSOSCFCL = true;
    oscillator2.enableROSC      = true;
    
    Board.InitPriority2 = "/ti/driverlib/GPIO";
    
    COMPARE1.$name               = "TIMER_Tm_100us32bit_MSW";
    COMPARE1.timerClkSrc         = "MFCLK";
    COMPARE1.timerPeriod         = 65536;
    COMPARE1.triggerSelect       = "Trigger";
    COMPARE1.subscriberPort      = "FSUB0";
    COMPARE1.subscriberChannel   = 1;
    COMPARE1.retentionRestoreCnt = true;
    COMPARE1.peripheral.$assign  = "TIMG7";
    
    GPIO1.$name                                       = "GPIO_LIN";
    GPIO1.associatedPins.create(2);
    GPIO1.associatedPins[0].$name                     = "EN";
    GPIO1.associatedPins[0].assignedPort              = "PORTA";
    GPIO1.associatedPins[0].assignedPin               = "7";
    GPIO1.associatedPins[1].$name                     = "RX";
    GPIO1.associatedPins[1].direction                 = "INPUT";
    GPIO1.associatedPins[1].assignedPort              = "PORTA";
    GPIO1.associatedPins[1].assignedPin               = "11";
    GPIO1.associatedPins[1].interruptEn               = true;
    GPIO1.associatedPins[1].polarity                  = "FALL";
    GPIO1.associatedPins[1].pin.$assignAllowConflicts = "PA11";
    
    GPIO2.$name                          = "GPIO_Diag";
    GPIO2.associatedPins.create(3);
    GPIO2.associatedPins[0].$name        = "VBATT_MEAS_EN";
    GPIO2.associatedPins[0].assignedPort = "PORTA";
    GPIO2.associatedPins[0].assignedPin  = "3";
    GPIO2.associatedPins[1].$name        = "TestPin0";
    GPIO2.associatedPins[1].assignedPort = "PORTA";
    GPIO2.associatedPins[1].assignedPin  = "5";
    GPIO2.associatedPins[2].$name        = "TestPin1";
    GPIO2.associatedPins[2].assignedPort = "PORTA";
    GPIO2.associatedPins[2].assignedPin  = "6";
    
    GPIO3.$name                          = "GPIO_Radar";
    GPIO3.associatedPins.create(4);
    GPIO3.associatedPins[0].$name        = "TRIG0";
    GPIO3.associatedPins[0].direction    = "INPUT";
    GPIO3.associatedPins[0].assignedPort = "PORTA";
    GPIO3.associatedPins[0].assignedPin  = "17";
    GPIO3.associatedPins[1].$name        = "TRIG1";
    GPIO3.associatedPins[1].direction    = "INPUT";
    GPIO3.associatedPins[1].assignedPort = "PORTA";
    GPIO3.associatedPins[1].assignedPin  = "22";
    GPIO3.associatedPins[1].interruptEn  = true;
    GPIO3.associatedPins[1].polarity     = "RISE";
    GPIO3.associatedPins[2].$name        = "TRIG2";
    GPIO3.associatedPins[2].direction    = "INPUT";
    GPIO3.associatedPins[2].assignedPort = "PORTA";
    GPIO3.associatedPins[2].assignedPin  = "24";
    GPIO3.associatedPins[2].interruptEn  = true;
    GPIO3.associatedPins[2].polarity     = "RISE";
    GPIO3.associatedPins[3].$name        = "TRIG3";
    GPIO3.associatedPins[3].assignedPort = "PORTA";
    GPIO3.associatedPins[3].assignedPin  = "25";
    GPIO3.associatedPins[3].direction    = "INPUT";
    
    GPIO4.$name                                       = "GPIO_Unused";
    GPIO4.associatedPins.create(10);
    GPIO4.associatedPins[0].$name                     = "PA0";
    GPIO4.associatedPins[0].assignedPort              = "PORTA";
    GPIO4.associatedPins[0].assignedPin               = "0";
    GPIO4.associatedPins[1].$name                     = "PA1";
    GPIO4.associatedPins[1].assignedPort              = "PORTA";
    GPIO4.associatedPins[1].assignedPin               = "1";
    GPIO4.associatedPins[2].$name                     = "PA4";
    GPIO4.associatedPins[2].assignedPort              = "PORTA";
    GPIO4.associatedPins[2].assignedPin               = "4";
    GPIO4.associatedPins[3].$name                     = "PA8";
    GPIO4.associatedPins[3].assignedPort              = "PORTA";
    GPIO4.associatedPins[3].assignedPin               = "8";
    GPIO4.associatedPins[3].pin.$assignAllowConflicts = "PA8";
    GPIO4.associatedPins[4].$name                     = "PA9";
    GPIO4.associatedPins[4].assignedPort              = "PORTA";
    GPIO4.associatedPins[4].assignedPin               = "9";
    GPIO4.associatedPins[4].pin.$assignAllowConflicts = "PA9";
    GPIO4.associatedPins[5].$name                     = "PA12";
    GPIO4.associatedPins[5].assignedPort              = "PORTA";
    GPIO4.associatedPins[5].assignedPin               = "12";
    GPIO4.associatedPins[6].$name                     = "PA13";
    GPIO4.associatedPins[6].assignedPort              = "PORTA";
    GPIO4.associatedPins[6].assignedPin               = "13";
    GPIO4.associatedPins[7].$name                     = "PA14";
    GPIO4.associatedPins[7].assignedPort              = "PORTA";
    GPIO4.associatedPins[7].assignedPin               = "14";
    GPIO4.associatedPins[8].$name                     = "PA26";
    GPIO4.associatedPins[8].assignedPort              = "PORTA";
    GPIO4.associatedPins[8].assignedPin               = "26";
    GPIO4.associatedPins[9].$name                     = "PA27";
    GPIO4.associatedPins[9].assignedPort              = "PORTA";
    GPIO4.associatedPins[9].assignedPin               = "27";
    
    SYSCTL.clockTreeEn = true;
    SYSCTL.powerPolicy = "STANDBY1";
    
    SYSTICK.periodEnable    = true;
    SYSTICK.period          = 32000;
    SYSTICK.interruptEnable = true;
    
    WWDT1.$name              = "WWDT0";
    WWDT1.clockDivider       = "8";
    WWDT1.periodCount        = "10";
    WWDT1.peripheral.$assign = "WWDT0";
    
    /**
     * Pinmux solution for unlocked pins/peripherals. This ensures that minor changes to the automatic solver in a future
     * version of the tool will not impact the pinmux you originally saw.  These lines can be completely deleted in order to
     * re-solve from scratch.
     */
    oscillator2.peripheral.$suggestSolution         = "SYSCTL";
    oscillator2.peripheral.roscPin.$suggestSolution = "PA2";
    Board.peripheral.$suggestSolution               = "DEBUGSS";
    Board.peripheral.swclkPin.$suggestSolution      = "PA20";
    Board.peripheral.swdioPin.$suggestSolution      = "PA19";
    GPIO1.associatedPins[0].pin.$suggestSolution    = "PA7";
    GPIO2.associatedPins[0].pin.$suggestSolution    = "PA3";
    GPIO2.associatedPins[1].pin.$suggestSolution    = "PA5";
    GPIO2.associatedPins[2].pin.$suggestSolution    = "PA6";
    GPIO3.associatedPins[0].pin.$suggestSolution    = "PA17";
    GPIO3.associatedPins[1].pin.$suggestSolution    = "PA22";
    GPIO3.associatedPins[2].pin.$suggestSolution    = "PA24";
    GPIO3.associatedPins[3].pin.$suggestSolution    = "PA25";
    GPIO4.associatedPins[0].pin.$suggestSolution    = "PA0";
    GPIO4.associatedPins[1].pin.$suggestSolution    = "PA1";
    GPIO4.associatedPins[2].pin.$suggestSolution    = "PA4";
    GPIO4.associatedPins[5].pin.$suggestSolution    = "PA12";
    GPIO4.associatedPins[6].pin.$suggestSolution    = "PA13";
    GPIO4.associatedPins[7].pin.$suggestSolution    = "PA14";
    GPIO4.associatedPins[8].pin.$suggestSolution    = "PA26";
    GPIO4.associatedPins[9].pin.$suggestSolution    = "PA27";
    

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Francois:

    非常感谢您对此事的通知。 您是对的;它是一个错误。 我们将在下一个 SDK 版本中修复它。

    此致、

    迭戈·阿巴德

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Diego:

    谢谢你。


    此致、
    François μ A。