This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC2640R2F:CC2640R2F:将代码从7X7至4x4。

Guru**** 1783250 points
Other Parts Discussed in Thread: CC2640R2F
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/1254628/cc2640r2f-cc2640r2f-move-the-code-from-7x7-to-4x4

器件型号:CC2640R2F

您好、TI!

由于我们使用4×4 RSM,所以我想将代码从2640R2F 7X7移动至4x4。


我参考以下文档步骤进行修改,但我认为2640R2F 仍然使用7X7电路板配置。

以下是我使用的步骤:
从现有的 CC2640R2_LAUNCHXL 复制现有的板级配置文件并重命名 CC2640R2DK_4XS
2.删除 CC2640R2_LAUNCHXL.c CC2640R2_LAUNCHXL.h
3.将 CC2640R2DK_4XS.c CC2640R2DK_4XS.h Board.h 从 \source\ti\ble5stack\boards\CC2640R2DK_4XS 导入 CC2640R2DK_4XS 文件。
4.修改中的 board.c 和 board.h \source\ti\ble5stack\target

为了验证2640R2F 是否 使用自定义板文件配置、因此我标记 CC2640R2_LAUNCHXL。
测试结果显示错误、未进入定制板级配置文件。

board.c

#if defined(CC2640R2DK_CXS) || defined (CC2640R2DK_4XS) \
      || defined (CC2640R2DK_5XD) ||  defined (CC2640R2DK_7ID)
    #include "./cc2640r2em/cc2640r2em_board.c"
//#elif defined(CC2640R2_LAUNCHXL)
    //#include "./cc2640r2lp/cc2640r2lp_board.c"
#elif defined(CC2640R2_RC)
    #include "./cc2640r2rc/cc2640r2rc_board.c"
#elif defined(CC26X2R1_LAUNCHXL)
    #include "./cc2652r1lp/cc2642r1lp_board.c"
#elif defined(CC13X2R1_LAUNCHXL)
    #include "./cc1352r1lp/cc1352r1lp_board.c"
#elif defined(CC2640R2DK_4XS)
    #include "../../boards/CC2640R2DK_4XS/Board.h"
    #include "../../boards/CC2640R2DK_4XS/CC2640R2DK_4XS.c"
#else // unknown board
    #error "***ERROR*** Invalid Board Specified! Please see board.h for options."
#endif

board.h

#if defined(CC2640R2DK_CXS) || defined (CC2640R2DK_4XS) \
      || defined (CC2640R2DK_5XD) ||  defined (CC2640R2DK_7ID)
    #include "./cc2640r2em/cc2640r2em_board.h"
//#elif defined(CC2640R2_LAUNCHXL)
    //#include "./cc2640r2lp/cc2640r2lp_board.h"
#elif defined(CC26X2R1_LAUNCHXL)
    #include "./cc2652r1lp/cc2642r1lp_board.h"
#elif defined(CC2640R2_RC)
    #include "./cc2640r2rc/cc2640r2rc_board.h"
#elif defined(CC13X2R1_LAUNCHXL)
    #include "./cc1352r1lp/cc1352r1lp_board.h"
#elif defined(CC2640R2DK_4XS)
    #include "../../boards/CC2640R2DK_4XS/Board.h" 
#else // unknown board
    #error "***ERROR*** Invalid Board Specified! Please see board.h for options."
#endif


此致、
迈克