This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CDCM9102:晶体要求

Guru**** 657500 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/clock-timing-group/clock-and-timing/f/clock-timing-forum/1199658/cdcm9102-crystal-requirement

器件型号:CDCM9102

您好、先生、

晶体是否具有规格要求?

我们使用的晶体规格为25MHz、+/-10ppm、DL 150uW、ESR<110 Ω

 ~调节电容 NC (C537)的晶体、容差为-6.5 μ F -9.5ppm、这是否满足要求? 谢谢。