This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] ADS1015:输入模拟电压容差

Guru**** 2515710 points
Other Parts Discussed in Thread: ADS1015

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/1014762/ads1015-input-analog-voltage-tolerance

器件型号:ADS1015

尊敬的:

由于采集模拟输入电压可能达到5V,我的设计板 VDD 为3.3V,但数据表显示 VDD±0.3V,最大值为3.6V < 5V (__LW_AT__可能会发生)所以您能帮我推广合适的 ADC,以满足我的设计要求。 平均值是模拟输入电压引脚 AIN0/1/2/3、希望它能够超过5V、您能帮助我像 ADS1015其他参数一样推广 ADC 吗?

注:如果将 VDD 电压更改为 5V,则我的 CPU 工作电压无法承受。