请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:DLPA3005 尊敬的:
我℃,DLPA3005的工作温度为0 ~70 ̊ C,但我想知道芯片是否可以 在-10℃(负10摄氏度),的温度下工作在这种情况下会发生什么?
它能正常工作吗? 或任何其他问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.