This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMUXHS4412:TMUXHS4412是否适用于独立的 PCIE4.0通道?

Guru**** 679710 points
Other Parts Discussed in Thread: TMUXHS4412
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1246950/tmuxhs4412-is-tmuxhs4412-suitable-for-the-pcie4-0-lanes-separate

器件型号:TMUXHS4412

我要求将4通道 PCIe 连接到两个连接器、一个是 PCIe 通道4、另一个是2通道。

因此,我用 TMUXHS4412进行如图所示的设计,绿色为4通道输入,红色为2通道输出,黄色为4通道输出。

我想确认一下这个设计是否可以正常工作,黄色信号是否会有性能问题,因为2通道黄色信号来自 TMUXHS4412 ,另外2通道直接与输入连接。