请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TCAN1042-Q1 主题中讨论的其他器件:TCAN1057A-Q1、TCAN1044A-Q1 、TCAN1057-Q1、
您好、专家:
客户希望在 TCAN1042和 TCAN1057之间实现兼容设计。 想要与您核实 TCAN1042的 PIN5 NC 是否可以连接5V?
谢谢!
温伊登
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好、专家:
客户希望在 TCAN1042和 TCAN1057之间实现兼容设计。 想要与您核实 TCAN1042的 PIN5 NC 是否可以连接5V?
谢谢!
温伊登