你(们)好
DRV83XX的产品名称是什么意思?
DRV830X:X数字按什么标准分类?
DRV83X2: X位的分类标准是什么?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你(们)好
DRV83XX的产品名称是什么意思?
DRV830X:X数字按什么标准分类?
DRV83X2: X位的分类标准是什么?
谢谢
您好,David:
我们的DRV830x和DRV83x2部件的命名有些模糊。 这些不应真正被视为"家庭",X没有真正的意义。
DRV830x栅极驱动器
DRV8300 = 100-V ABS最大栅极驱动器,高达1.5A的汇栅极电流,自2020年起
DRV8301/2/3 = 60 V ABS最大栅极驱动器,从2011-2013年2013年起高达2.3A的汇栅电流
DRV8304 = 40 V ABS最大栅极驱动器,高达2A汇门电流,自2017年起
DRV8305/-Q1 = 40V ABS最大栅极驱动器,从2015年起提供高达1A的汇栅电流,工业级和自动级0
DRV8306 = 40 V ABS最大栅极驱动器,带感应梯形控制,0.3A汇电流,自2018年起
DRV8307/DRV8308 =8308 = 40 V ABS最大梯形和正弦控制栅极驱动器,自2014年起高达30/130mA栅极驱动电流
DRV83x2集成MOSFET驱动器
DRV8312 = 70 V ABS最大驱动器,高达6.5A峰值电流,自2010年起
DRV8332 = 70 V ABS最大驱动器,高达13A峰值电流,自2010年起
希望这能有所帮助,
亚伦