Other Parts Discussed in Thread: MSP430FR2433
我正在使用示例 TIMER_A_ex2_ContinousModeOperationWithCCR0Interrupt 尝试在 P1.0上生成 PWM 信号。
每当我运行程序时、P1.0都会在一段时间后变为高电平、但从不会产生 PWM 信号。
我已经试着修改代码一些以获得 PWM 信号、但到目前为止没成功。
下面是代码:
/* --COPYRIGHT--,BSD
* Copyright (c) 2017, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
* --/COPYRIGHT--*/
//******************************************************************************
//! TIMER_A, Toggle LED1, CCR0 Cont. Mode ISR, DCO SMCLK
//!
//! Toggle LED1 using software and TA_0 ISR. Toggles every
//! 50000 SMCLK cycles. SMCLK provides clock source for TACLK.
//! During the TA_0 ISR, LED1 is toggled and 50000 clock cycles are added to
//! CCR0. TA_0 ISR is triggered every 50000 cycles. CPU is normally off and
//! used only during TA_ISR.
//! ACLK = n/a, MCLK = SMCLK = TACLK = default DCO ~1.048MHz
//!
//! MSP430FR2xx_4xx Board
//! ---------------
//! /|\| |
//! | | |
//! --|RST |
//! | |
//! | |-->LED1
//!
//! This example uses the following peripherals and I/O signals. You must
//! review these and change as needed for your own board:
//! - TimerA peripheral
//! - GPIO peripheral
//!
//! This example uses the following interrupt handlers. To use this example
//! in your own application you must add these interrupt handlers to your
//! vector table.
//! - Timer A0
//!
//*****************************************************************************
#include "driverlib.h"
#include "Board.h"
#define COMPARE_VALUE 50000
void main (void)
{
//Stop Watchdog Timer
WDT_A_hold(WDT_A_BASE);
//Set LED1 as an output pin.
GPIO_setAsOutputPin(
GPIO_PORT_P1,
GPIO_PIN0
);
/*
* Disable the GPIO power-on default high-impedance mode to activate
* previously configured port settings
*/
PMM_unlockLPM5();
//Start timer in continuous mode sourced by SMCLK
Timer_A_initContinuousModeParam initContParam = {0};
initContParam.clockSource = TIMER_A_CLOCKSOURCE_SMCLK;
initContParam.clockSourceDivider = TIMER_A_CLOCKSOURCE_DIVIDER_1;
initContParam.timerInterruptEnable_TAIE = TIMER_A_TAIE_INTERRUPT_DISABLE;
initContParam.timerClear = TIMER_A_DO_CLEAR;
initContParam.startTimer = false;
Timer_A_initContinuousMode(TIMER_A1_BASE, &initContParam);
//Initiaze compare mode
Timer_A_clearCaptureCompareInterrupt(TIMER_A1_BASE,
TIMER_A_CAPTURECOMPARE_REGISTER_0
);
Timer_A_initCompareModeParam initCompParam = {0};
initCompParam.compareRegister = TIMER_A_CAPTURECOMPARE_REGISTER_0;
initCompParam.compareInterruptEnable = TIMER_A_CAPTURECOMPARE_INTERRUPT_ENABLE;
initCompParam.compareOutputMode = TIMER_A_OUTPUTMODE_OUTBITVALUE;
initCompParam.compareValue = COMPARE_VALUE;
Timer_A_initCompareMode(TIMER_A1_BASE, &initCompParam);
Timer_A_startCounter( TIMER_A1_BASE,
TIMER_A_CONTINUOUS_MODE
);
//Enter LPM0, enable interrupts
//__bis_SR_register(LPM0_bits + GIE);
//For debugger
//__no_operation();
}
//******************************************************************************
//
//This is the TIMER1_A0 interrupt vector service routine.
//
//******************************************************************************
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=TIMER1_A0_VECTOR
__interrupt
#elif defined(__GNUC__)
__attribute__((interrupt(TIMER1_A0_VECTOR)))
#endif
void TIMER1_A0_ISR (void)
{
uint16_t compVal = Timer_A_getCaptureCompareCount(TIMER_A1_BASE,
TIMER_A_CAPTURECOMPARE_REGISTER_0)
+ COMPARE_VALUE;
//Toggle LED1
GPIO_toggleOutputOnPin(
GPIO_PORT_P1,
GPIO_PIN0
);
//Add Offset to CCR0
//Timer_A_setCompareValue(TIMER_A1_BASE,
// TIMER_A_CAPTURECOMPARE_REGISTER_0,
// compVal
// );
// Reset timer
//Timer_A_clear(TIMER_A1_BASE);
//Timer_A_clearCaptureCompareInterrupt(TIMER_A1_BASE, TIMER_A_CAPTURECOMPARE_REGISTER_0);
Timer_A_clearTimerInterrupt(TIMER_A1_BASE);
}