This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AM3352:"警告:可疑的 RCU 使用和 quot;在 dmesg 中

Guru**** 670150 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1129785/am3352-warning-suspicious-rcu-usage-in-dmesg

器件型号:AM3352
主题中讨论的其他器件:ADS7846BQ24190TWL6040DRA752TPS65023TPS62360TPS65218BQ24735TMP102TPS65217TSC2005TPS65910TSC2007

我 在 编译 ti-linux-kernel v08.04.04.01.002 (基于 v5.10.136)时遇到以下错误、除 defconfig 和 dts 之外、未进行任何修改。  硬件是一款与 EVM 设计非常相似的 Olimex AM3352-SOM。

[  154.843094] omap_intc_handle_irq: spurious irq!

[  154.850046] =============================
[  154.850064] WARNING: suspicious RCU usage
[  154.850082] 5.10.136-00001-geeddd634953 #9 Not tainted
[  154.850099] -----------------------------
[  154.850118] ./include/trace/events/lock.h:37 suspicious rcu_dereference_check() usage!

[  154.850148] other info that might help us debug this:


[  154.850191] rcu_scheduler_active = 2, debug_locks = 1
[  154.850209] RCU used illegally from extended quiescent state!
[  154.850225] no locks held by swapper/0/0.

[  154.850253] stack backtrace:
[  154.850272] CPU: 0 PID: 0 Comm: swapper/0 Not tainted 5.10.136-00001-geeddd634953 #9
[  154.850289] Hardware name: Generic AM33XX (Flattened Device Tree)
[  154.850308] [<c01110c8>] (unwind_backtrace) from [<c010c118>] (show_stack+0x10/0x14)
[  154.850326] [<c010c118>] (show_stack) from [<c0a4ff48>] (dump_stack+0xe0/0x10c)
[  154.850344] [<c0a4ff48>] (dump_stack) from [<c01affc8>] (lock_acquire+0x304/0x444)
[  154.850363] [<c01affc8>] (lock_acquire) from [<c0a5d270>] (_raw_spin_lock+0x40/0x50)
[  154.850382] [<c0a5d270>] (_raw_spin_lock) from [<c01bc808>] (vprintk_emit+0x5c/0x2dc)
[  154.850400] [<c01bc808>] (vprintk_emit) from [<c01bcaa8>] (vprintk_default+0x20/0x28)
[  154.850418] [<c01bcaa8>] (vprintk_default) from [<c0a4c94c>] (printk+0x2c/0x54)
[  154.850436] [<c0a4c94c>] (printk) from [<c0643128>] (omap_intc_handle_irq+0x74/0x90)
[  154.850456] [<c0643128>] (omap_intc_handle_irq) from [<c0100b70>] (__irq_svc+0x70/0x98)
[  154.850472] Exception stack(0xc1001f10 to 0xc1001f58)
[  154.850491] 1f00:                                     ffffffff ffffffff 00000001 c011c3a0
[  154.850510] 1f20: c1109ce0 c1009254 00000001 c100929c 00000000 00000000 c1009208 c10092b4
[  154.850527] 1f40: c1000000 c1001f60 c0108634 c0108638 60010013 ffffffff
[  154.850546] [<c0100b70>] (__irq_svc) from [<c0108638>] (arch_cpu_idle+0x30/0x3c)
[  154.850564] [<c0108638>] (arch_cpu_idle) from [<c0a5cff0>] (default_idle_call+0x78/0x2b8)
[  154.850583] [<c0a5cff0>] (default_idle_call) from [<c017b548>] (do_idle+0x1d4/0x2b4)
[  154.850601] [<c017b548>] (do_idle) from [<c017b9fc>] (cpu_startup_entry+0x18/0x1c)
[  154.850620] [<c017b9fc>] (cpu_startup_entry) from [<c0f00f68>] (start_kernel+0x488/0x568)

DTS:

/*
 * Copyright (C) 2012 Texas Instruments Incorporated - http://www.ti.com/
 *
 * This program is free software; you can redistribute it and/or modify
 * it under the terms of the GNU General Public License version 2 as
 * published by the Free Software Foundation.
 */
/dts-v1/;

#include "am33xx.dtsi"
#include <dt-bindings/pwm/pwm.h>
#include <dt-bindings/interrupt-controller/irq.h>

/ {
	model = "OLIMEX AM335x-SOM VoltServer ETX8";
	compatible = "olimex,am335x_som", "ti,am33xx";

	chosen {
		stdout-path = &uart0;
		tick-timer = &timer2;
	};

	leds: leds {
		compatible = "gpio-leds";
	};

	gpio_keys: gpio_keys {
		compatible = "gpio-keys";
	};

	memory {
		device_type = "memory";
		reg = <0x80000000 0x20000000>; /* 512 MB */
	};

	dummy_reg: regulator@0 {
		compatible = "regulator-fixed";
		regulator-name = "dummy_regulator";
		regulator-min-microvolt = <3300000>;
		regulator-max-microvolt = <3300000>;
	};
};

&leds {
	pinctrl-names = "default";
	pinctrl-0 = <&usr_led_pins_default>, <&evb_leds_pins_default>;

	led@0 {
		label = "olimex-som:green:led1";
		gpios = <&gpio3 18 GPIO_ACTIVE_HIGH>;
		linux,default-trigger = "heartbeat";
		default-state = "off";
	};

	led@1 {
		label = "etx8:blue:led2"; // red on the Olimex EVB
		gpios = <&gpio3 20 GPIO_ACTIVE_HIGH>;
		linux,default-trigger = "none"; // "mmc0"
		default-state = "off";
	};

	led@2 {
		label = "etx8:green:led3"; // yellow on the Olimex EVB
		gpios = <&gpio3 21 GPIO_ACTIVE_HIGH>;
		linux,default-trigger = "heartbeat"; // "cpu0"
		default-state = "off";
	};
};
&am33xx_pinmux {
	usr_led_pins_default: usr_led_pins_default {
		pinctrl-single,pins = <
			AM33XX_PADCONF(AM335X_PIN_MCASP0_ACLKR, PIN_OUTPUT, MUX_MODE7) /* (B12) gpio3_18 */
			/* 0x1a0 ( PIN_OUTPUT | MUX_MODE7 ) /* (B12) mcasp0_aclkr.gpio3_18 */
		>;
	};

	evb_leds_pins_default: evb_leds_pins_default {
		pinctrl-single,pins = <
			AM33XX_PADCONF(AM335X_PIN_MCASP0_AXR1, PIN_OUTPUT, MUX_MODE7) /* (D13) mcasp0_axr1.gpio3_20 */
			AM33XX_PADCONF(AM335X_PIN_MCASP0_AHCLKX, PIN_OUTPUT, MUX_MODE7) /* (A14) mcasp0_ahclkx.gpio3_21 */
			/* 0x1a8 ( PIN_OUTPUT | MUX_MODE7 ) /* (D13) mcasp0_axr1.gpio3_20 */
			/* 0x1ac ( PIN_OUTPUT | MUX_MODE7 ) /* (A14) mcasp0_ahclkx.gpio3_21 */
		>;
	};
};

&gpio_keys {
	label = "gpio keys";

	factory_reset {
		label = "Factory RESET";
		linux,code = <87>; /* F11 key */
		gpios = <&gpio3 19 GPIO_ACTIVE_LOW>; // pin 35 on AM_CON-LCD header
		/* Note: dmesg will show an error "omap_gpio 44e07000.gpio: Could not set line 19 debounce to 50000 microseconds (-22)"
		  However the gpio-keys driver will use software debounce instead.  The max hw debounce is 7.9 ms */
		debounce-interval = <50>;
	};
};
&am33xx_pinmux {
	pinctrl-0 = <&gpio3_pins>;
	gpio3_pins: pinmux_gpio3_pins {
		pinctrl-single,pins = <
			AM33XX_PADCONF(AM335X_PIN_MCASP0_FSR, PIN_INPUT_PULLUP, MUX_MODE7) /* (C13) gpio3_19 */
			/* 0x1e4 (PIN_INPUT_PULLUP | MUX_MODE7) /* (C13) emu0.gpio3_19 */
			/*0x1e4 (PIN_INPUT_PULLUP | MUX_MODE7) /* (C14) emu0.gpio3_7 */
			/*0x1e8 (PIN_INPUT_PULLUP | MUX_MODE7) /* (B14) emu1.gpio3_8 */
		>;
	};
};


&uart0 {
	pinctrl-names = "default";
	pinctrl-0 = <&uart0_pins>;
	status = "okay";
};
&am33xx_pinmux {
	uart0_pins: uart0_pins_default {
		pinctrl-single,pins = <
			AM33XX_PADCONF(AM335X_PIN_UART0_RXD, PIN_INPUT_PULLUP, MUX_MODE0)
			AM33XX_PADCONF(AM335X_PIN_UART0_TXD, PIN_OUTPUT_PULLDOWN, MUX_MODE0)
		>;
	};
};

&uart1 {
	pinctrl-names = "default";
	pinctrl-0 = <&uart1_pins>;
	status = "okay";
};
&am33xx_pinmux {
	uart1_pins: pinmux_uart1_pins {
		pinctrl-single,pins = <
			AM33XX_PADCONF(AM335X_PIN_UART1_RXD, PIN_INPUT_PULLUP, MUX_MODE0)
			AM33XX_PADCONF(AM335X_PIN_UART1_TXD, PIN_OUTPUT_PULLDOWN, MUX_MODE0)
		>;
	};
};

&uart4 {
	pinctrl-names = "default";
	pinctrl-0 = <&uart4_pins>;
	status = "disabled";
};
&am33xx_pinmux {
	uart4_pins: pinmux_uart4_pins {
		pinctrl-single,pins = <
			AM33XX_PADCONF(AM335X_PIN_UART0_CTSN, PIN_INPUT_PULLUP, MUX_MODE1) /* (E18) uart0_ctsn.uart4_rxd */
			AM33XX_PADCONF(AM335X_PIN_UART0_RTSN, PIN_OUTPUT, MUX_MODE1) /* (E17) uart0_rtsn.uart4_txd */
			/* 0x168 ( PIN_INPUT_PULLUP | MUX_MODE1 ) /* (E18) uart0_ctsn.uart4_rxd */
			/* 0x16c ( PIN_OUTPUT | MUX_MODE1 ) /* (E17) uart0_rtsn.uart4_txd */
		>;
	};
};

&mmc1 {
	status = "okay";
	bus-width = <0x4>;
	pinctrl-names = "default";
	pinctrl-0 = <&mmc1_pins>;
	cd-gpios = <&gpio0 6 GPIO_ACTIVE_HIGH>;
	cd-inverted;
	vmmc-supply = <&dummy_reg>;
};
&am33xx_pinmux {
	mmc1_pins: pinmux_mmc1_pins {
		pinctrl-single,pins = <
			AM33XX_PADCONF(AM335X_PIN_SPI0_CS1, PIN_INPUT, MUX_MODE7)		/* spi0_cs1.gpio0_6 */
			AM33XX_PADCONF(AM335X_PIN_MMC0_DAT0, PIN_INPUT_PULLUP, MUX_MODE0)
			AM33XX_PADCONF(AM335X_PIN_MMC0_DAT1, PIN_INPUT_PULLUP, MUX_MODE0)
			AM33XX_PADCONF(AM335X_PIN_MMC0_DAT2, PIN_INPUT_PULLUP, MUX_MODE0)
			AM33XX_PADCONF(AM335X_PIN_MMC0_DAT3, PIN_INPUT_PULLUP, MUX_MODE0)
			AM33XX_PADCONF(AM335X_PIN_MMC0_CMD, PIN_INPUT_PULLUP, MUX_MODE0)
			AM33XX_PADCONF(AM335X_PIN_MMC0_CLK, PIN_INPUT_PULLUP, MUX_MODE0)
		>;
	};
};

&mac {
	pinctrl-names = "default";
	pinctrl-0 = <&cpsw1_pins>; /*, <&cpsw2_pins>; */
	status = "okay";
	/* dual_emac = <1>; */
	slaves = <1>;
};
&am33xx_pinmux {
	/* Refer to LAN8710A 00002164B.pdf table 2-1, p7 */
	cpsw1_pins: pinmux_cpsw1 {
		pinctrl-single,pins = <
			AM33XX_PADCONF(AM335X_PIN_MII1_TX_EN, PIN_OUTPUT_PULLDOWN, MUX_MODE0)	/* mii1_txen.rgmii1_tctl */
			AM33XX_PADCONF(AM335X_PIN_MII1_RX_DV, PIN_INPUT_PULLUP, MUX_MODE0)	/* mii1_rxdv.rgmii1_rctl */
			AM33XX_PADCONF(AM335X_PIN_MII1_TXD3, PIN_OUTPUT_PULLDOWN, MUX_MODE0)	/* mii1_txd3.rgmii1_td3 */
			AM33XX_PADCONF(AM335X_PIN_MII1_TXD2, PIN_OUTPUT_PULLDOWN, MUX_MODE0)	/* mii1_txd2.rgmii1_td2 */
			AM33XX_PADCONF(AM335X_PIN_MII1_TXD1, PIN_OUTPUT_PULLDOWN, MUX_MODE0)	/* mii1_txd1.rgmii1_td1 */
			AM33XX_PADCONF(AM335X_PIN_MII1_TXD0, PIN_OUTPUT_PULLDOWN, MUX_MODE0)	/* mii1_txd0.rgmii1_td0 */
			AM33XX_PADCONF(AM335X_PIN_MII1_TX_CLK, PIN_INPUT_PULLUP, MUX_MODE0)	/* mii1_txclk.rgmii1_tclk */
			AM33XX_PADCONF(AM335X_PIN_MII1_RX_CLK, PIN_INPUT_PULLUP, MUX_MODE0)	/* mii1_rxclk.rgmii1_rclk */
			AM33XX_PADCONF(AM335X_PIN_MII1_RXD3, PIN_INPUT_PULLUP, MUX_MODE0)	/* mii1_rxd3.rgmii1_rd3 */
			AM33XX_PADCONF(AM335X_PIN_MII1_RXD2, PIN_INPUT_PULLUP, MUX_MODE0)	/* mii1_rxd2.rgmii1_rd2 */
			AM33XX_PADCONF(AM335X_PIN_MII1_RXD1, PIN_INPUT_PULLUP, MUX_MODE0)	/* mii1_rxd1.rgmii1_rd1 */
			AM33XX_PADCONF(AM335X_PIN_MII1_RXD0, PIN_INPUT_PULLUP, MUX_MODE0)	/* mii1_rxd0.rgmii1_rd0 */
			AM33XX_PADCONF(AM335X_PIN_MII1_RX_ER, PIN_INPUT_PULLUP, MUX_MODE0)	/* (J15) gmii1_rxer.gmii1_rxer */

			AM33XX_PADCONF(AM335X_PIN_MII1_COL, PIN_INPUT, MUX_MODE0)	/* (H16) mii1_col.gpio3_0 */
			AM33XX_PADCONF(AM335X_PIN_MII1_CRS, PIN_INPUT_PULLDOWN, MUX_MODE0)	/* (H17) gmii1_crs.gmii1_crs */
		>;
	};

	cpsw2_pins: pinmux_cpsw2 {
		pinctrl-single,pins = <
			/* 0x78 ( PIN_INPUT | MUX_MODE1 ) /* (U18) gpmc_be1n.gmii2_col */
			/* 0x70 ( PIN_INPUT | MUX_MODE1 ) /* (T17) gpmc_wait0.gmii2_crs */
			/* 0x74 ( PIN_INPUT_PULLUP | MUX_MODE1 ) /* (U17) gpmc_wpn.gmii2_rxer */
			AM33XX_PADCONF(AM335X_PIN_GPMC_BEN1, PIN_INPUT, MUX_MODE1)	/* (U18) gpmc_be1n.gmii2_col */
			AM33XX_PADCONF(AM335X_PIN_GPMC_WAIT0, PIN_INPUT, MUX_MODE1)	/* (T17) gpmc_wait0.gmii2_crs */
			AM33XX_PADCONF(AM335X_PIN_GPMC_WPN, PIN_INPUT_PULLUP, MUX_MODE1)	/* (U17) gpmc_wpn.gmii2_rxer */

			AM33XX_PADCONF(AM335X_PIN_GPMC_A0, PIN_OUTPUT_PULLDOWN, MUX_MODE1)	/* gpmc_a0.rgmii2_tctl */
			AM33XX_PADCONF(AM335X_PIN_GPMC_A1, PIN_INPUT_PULLDOWN, MUX_MODE1)	/* gpmc_a1.rgmii2_rctl */
			AM33XX_PADCONF(AM335X_PIN_GPMC_A2, PIN_OUTPUT_PULLDOWN, MUX_MODE1)	/* gpmc_a2.rgmii2_td3 */
			AM33XX_PADCONF(AM335X_PIN_GPMC_A3, PIN_OUTPUT_PULLDOWN, MUX_MODE1)	/* gpmc_a3.rgmii2_td2 */
			AM33XX_PADCONF(AM335X_PIN_GPMC_A4, PIN_OUTPUT_PULLDOWN, MUX_MODE1)	/* gpmc_a4.rgmii2_td1 */
			AM33XX_PADCONF(AM335X_PIN_GPMC_A5, PIN_OUTPUT_PULLDOWN, MUX_MODE1)	/* gpmc_a5.rgmii2_td0 */
			AM33XX_PADCONF(AM335X_PIN_GPMC_A6, PIN_OUTPUT_PULLDOWN, MUX_MODE1)	/* gpmc_a6.rgmii2_tclk */
			AM33XX_PADCONF(AM335X_PIN_GPMC_A7, PIN_INPUT_PULLDOWN, MUX_MODE1)	/* gpmc_a7.rgmii2_rclk */
			AM33XX_PADCONF(AM335X_PIN_GPMC_A8, PIN_INPUT_PULLDOWN, MUX_MODE1)	/* gpmc_a8.rgmii2_rd3 */
			AM33XX_PADCONF(AM335X_PIN_GPMC_A9, PIN_INPUT_PULLDOWN, MUX_MODE1)	/* gpmc_a9.rgmii2_rd2 */
			AM33XX_PADCONF(AM335X_PIN_GPMC_A10, PIN_INPUT_PULLDOWN, MUX_MODE1)	/* gpmc_a10.rgmii2_rd1 */
			AM33XX_PADCONF(AM335X_PIN_GPMC_A11, PIN_INPUT_PULLDOWN, MUX_MODE1)	/* gpmc_a11.rgmii2_rd0 */
		>;
	};
};

&davinci_mdio {
	pinctrl-names = "default"; //, "sleep";
	pinctrl-0 = <&davinci_mdio_pins>;
	status = "okay";
	reset-gpios = <&gpio0 29 GPIO_ACTIVE_LOW>;
	reset-delay-us = <25000>; /* LAN8710A 00002164B.pdf table 5-7, p60 */

	ethphy0: ethernet-phy@0 {
		reg = <0>;
	};
	/*
	ethphy1: ethernet-phy@1 {
		reg = <1>;
	};
	*/
};
&am33xx_pinmux {
	/* Refer to LAN8710A 00002164B.pdf table 2-3, p12 */
	davinci_mdio_pins: pinmux_davinci_mdio {
		pinctrl-single,pins = <
			AM33XX_PADCONF(AM335X_PIN_MDIO, PIN_INPUT_PULLUP | SLEWCTRL_FAST, MUX_MODE0)
			AM33XX_PADCONF(AM335X_PIN_MDC, PIN_OUTPUT_PULLUP, MUX_MODE0)
			AM33XX_PADCONF(AM335X_PIN_RMII1_REF_CLK, PIN_INPUT_PULLUP, MUX_MODE7)	/* rmii2_refclk.gpio0_29 */
		>;
	};
};

&cpsw_emac0 {
	phy-handle = <&ethphy0>;
	phy-mode = "mii";
	/* dual_emac_res_vlan = <1>; */
};
/*
&cpsw_emac1 {
	phy-handle = <&ethphy1>;
	phy-mode = "mii";
	dual_emac_res_vlan = <2>;
};
*/

&sham {
	status = "okay";
};

&aes {
	status = "okay";
};

&rtc {
	clocks = <&clk_32768_ck>, <&clk_24mhz_clkctrl AM3_CLK_24MHZ_CLKDIV32K_CLKCTRL 0>;
	clock-names = "ext-clk", "int-clk";
};

defconfig:

CONFIG_KERNEL_LZO=y
CONFIG_DEFAULT_HOSTNAME="etx8"
CONFIG_SYSVIPC=y
CONFIG_POSIX_MQUEUE=y
CONFIG_AUDIT=y
CONFIG_NO_HZ=y
CONFIG_HIGH_RES_TIMERS=y
CONFIG_BSD_PROCESS_ACCT=y
CONFIG_IKCONFIG=y
CONFIG_IKCONFIG_PROC=y
CONFIG_LOG_BUF_SHIFT=16
CONFIG_CGROUPS=y
CONFIG_MEMCG=y
CONFIG_BLK_CGROUP=y
CONFIG_CGROUP_SCHED=y
CONFIG_CFS_BANDWIDTH=y
CONFIG_RT_GROUP_SCHED=y
CONFIG_CGROUP_FREEZER=y
CONFIG_CPUSETS=y
CONFIG_CGROUP_DEVICE=y
CONFIG_CGROUP_CPUACCT=y
CONFIG_CGROUP_PERF=y
CONFIG_NAMESPACES=y
CONFIG_BLK_DEV_INITRD=y
CONFIG_EXPERT=y
# CONFIG_COMPAT_BRK is not set
CONFIG_SLAB=y
CONFIG_PROFILING=y
CONFIG_ARCH_MULTI_V6=y
CONFIG_POWER_AVS_OMAP=y
CONFIG_POWER_AVS_OMAP_CLASS3=y
CONFIG_OMAP_RESET_CLOCKS=y
CONFIG_ARCH_OMAP2=y
CONFIG_ARCH_OMAP3=y
CONFIG_ARCH_OMAP4=y
CONFIG_SOC_OMAP5=y
CONFIG_SOC_AM33XX=y
CONFIG_SOC_AM43XX=y
CONFIG_SOC_DRA7XX=y
CONFIG_ARM_THUMBEE=y
CONFIG_ARM_ERRATA_411920=y
CONFIG_SMP=y
CONFIG_NR_CPUS=2
CONFIG_ARM_APPENDED_DTB=y
CONFIG_ARM_ATAG_DTB_COMPAT=y
CONFIG_CMDLINE="root=/dev/mmcblk0p1 rootwait console=ttyS0,115200"
CONFIG_KEXEC=y
CONFIG_CPU_FREQ=y
CONFIG_CPU_FREQ_DEFAULT_GOV_ONDEMAND=y
CONFIG_CPU_FREQ_GOV_POWERSAVE=y
CONFIG_CPU_FREQ_GOV_USERSPACE=y
CONFIG_CPU_FREQ_GOV_CONSERVATIVE=y
CONFIG_CPUFREQ_DT=m
CONFIG_CPU_IDLE=y
CONFIG_KERNEL_MODE_NEON=y
CONFIG_PM_DEBUG=y
CONFIG_CRYPTO_SHA1_ARM_NEON=m
CONFIG_CRYPTO_SHA256_ARM=m
CONFIG_CRYPTO_SHA512_ARM=m
CONFIG_CRYPTO_AES_ARM=m
CONFIG_CRYPTO_AES_ARM_BS=m
CONFIG_CRYPTO_CRC32_ARM_CE=m
CONFIG_OPROFILE=y
CONFIG_KPROBES=y
CONFIG_MODULES=y
CONFIG_MODULE_FORCE_LOAD=y
CONFIG_MODULE_UNLOAD=y
CONFIG_MODULE_FORCE_UNLOAD=y
CONFIG_MODVERSIONS=y
CONFIG_MODULE_SRCVERSION_ALL=y
# CONFIG_BLK_DEV_BSG is not set
CONFIG_PARTITION_ADVANCED=y
CONFIG_BINFMT_MISC=y
CONFIG_CMA=y
CONFIG_NET=y
CONFIG_PACKET=y
CONFIG_UNIX=y
CONFIG_XFRM_USER=y
CONFIG_NET_KEY=y
CONFIG_NET_KEY_MIGRATE=y
CONFIG_INET=y
CONFIG_IP_MULTICAST=y
CONFIG_IP_PNP=y
CONFIG_IP_PNP_DHCP=y
CONFIG_IP_PNP_BOOTP=y
CONFIG_IP_PNP_RARP=y
CONFIG_NET_IPIP=m
CONFIG_NETFILTER=y
CONFIG_NETFILTER_NETLINK_LOG=m
CONFIG_NF_CONNTRACK=m
CONFIG_NF_CONNTRACK_ZONES=y
# CONFIG_NF_CONNTRACK_PROCFS is not set
CONFIG_NF_CONNTRACK_EVENTS=y
CONFIG_NF_CONNTRACK_TIMEOUT=y
CONFIG_NF_CONNTRACK_TIMESTAMP=y
CONFIG_NF_CONNTRACK_SNMP=m
CONFIG_NF_CT_NETLINK=m
CONFIG_NF_CT_NETLINK_TIMEOUT=m
CONFIG_NETFILTER_NETLINK_GLUE_CT=y
CONFIG_NF_TABLES=m
CONFIG_NF_TABLES_INET=y
CONFIG_NF_TABLES_NETDEV=y
CONFIG_NFT_CT=m
CONFIG_NFT_COUNTER=m
CONFIG_NFT_CONNLIMIT=m
CONFIG_NFT_LOG=m
CONFIG_NFT_LIMIT=m
CONFIG_NFT_MASQ=m
CONFIG_NFT_REDIR=m
CONFIG_NFT_NAT=m
CONFIG_NFT_OBJREF=m
CONFIG_NFT_REJECT=m
CONFIG_NFT_COMPAT=m
CONFIG_NFT_HASH=m
CONFIG_NFT_DUP_NETDEV=m
CONFIG_NFT_FWD_NETDEV=m
CONFIG_NETFILTER_XT_TARGET_CONNMARK=m
CONFIG_NETFILTER_XT_TARGET_CT=m
CONFIG_NETFILTER_XT_TARGET_LED=m
CONFIG_NETFILTER_XT_TARGET_LOG=m
CONFIG_NETFILTER_XT_TARGET_MARK=m
CONFIG_NETFILTER_XT_MATCH_ADDRTYPE=m
CONFIG_NETFILTER_XT_MATCH_COMMENT=m
CONFIG_NETFILTER_XT_MATCH_CONNBYTES=m
CONFIG_NETFILTER_XT_MATCH_CONNLABEL=m
CONFIG_NETFILTER_XT_MATCH_CONNLIMIT=m
CONFIG_NETFILTER_XT_MATCH_CONNMARK=m
CONFIG_NETFILTER_XT_MATCH_CONNTRACK=m
CONFIG_NETFILTER_XT_MATCH_CPU=m
CONFIG_NETFILTER_XT_MATCH_IPRANGE=m
# CONFIG_NETFILTER_XT_MATCH_L2TP is not set
CONFIG_NETFILTER_XT_MATCH_LENGTH=m
CONFIG_NETFILTER_XT_MATCH_LIMIT=m
CONFIG_NETFILTER_XT_MATCH_MAC=m
CONFIG_NETFILTER_XT_MATCH_MARK=m
CONFIG_NETFILTER_XT_MATCH_MULTIPORT=m
CONFIG_NETFILTER_XT_MATCH_OWNER=m
CONFIG_NETFILTER_XT_MATCH_PKTTYPE=m
CONFIG_NETFILTER_XT_MATCH_RECENT=m
CONFIG_NETFILTER_XT_MATCH_SOCKET=m
CONFIG_NETFILTER_XT_MATCH_STATE=m
CONFIG_NETFILTER_XT_MATCH_STATISTIC=m
CONFIG_NETFILTER_XT_MATCH_TIME=m
CONFIG_IP_SET=m
CONFIG_IP_SET_BITMAP_IP=m
CONFIG_IP_SET_BITMAP_IPMAC=m
CONFIG_IP_SET_BITMAP_PORT=m
CONFIG_IP_SET_HASH_IP=m
CONFIG_IP_SET_HASH_IPMARK=m
CONFIG_IP_SET_HASH_IPPORT=m
CONFIG_IP_SET_HASH_IPPORTIP=m
CONFIG_IP_SET_HASH_IPPORTNET=m
CONFIG_IP_SET_HASH_MAC=m
CONFIG_IP_SET_HASH_NETPORTNET=m
CONFIG_IP_SET_HASH_NET=m
CONFIG_IP_SET_HASH_NETNET=m
CONFIG_IP_SET_HASH_NETPORT=m
CONFIG_IP_SET_HASH_NETIFACE=m
CONFIG_IP_SET_LIST_SET=m
CONFIG_IP_NF_IPTABLES=m
CONFIG_IP_NF_MATCH_RPFILTER=m
CONFIG_IP_NF_MATCH_TTL=m
CONFIG_IP_NF_FILTER=m
CONFIG_IP_NF_TARGET_REJECT=m
CONFIG_IP_NF_TARGET_SYNPROXY=m
CONFIG_IP_NF_NAT=m
CONFIG_IP_NF_TARGET_MASQUERADE=m
CONFIG_IP_NF_TARGET_NETMAP=m
CONFIG_IP_NF_TARGET_REDIRECT=m
CONFIG_IP_NF_MANGLE=m
CONFIG_IP_NF_TARGET_TTL=m
CONFIG_IP_NF_RAW=m
CONFIG_IP_NF_SECURITY=m
CONFIG_IP6_NF_IPTABLES=m
CONFIG_IP6_NF_MATCH_FRAG=m
CONFIG_IP6_NF_MATCH_RPFILTER=m
CONFIG_IP6_NF_FILTER=m
CONFIG_IP6_NF_TARGET_REJECT=m
CONFIG_IP6_NF_TARGET_SYNPROXY=m
CONFIG_IP6_NF_MANGLE=m
CONFIG_IP6_NF_RAW=m
CONFIG_IP6_NF_SECURITY=m
CONFIG_IP6_NF_NAT=m
CONFIG_IP6_NF_TARGET_MASQUERADE=m
CONFIG_IP6_NF_TARGET_NPT=m
CONFIG_L2TP=m
CONFIG_VLAN_8021Q=m
CONFIG_VLAN_8021Q_GVRP=y
CONFIG_NETLINK_DIAG=m
CONFIG_BPF_JIT=y
CONFIG_CAN=m
CONFIG_CAN_C_CAN=m
CONFIG_CAN_C_CAN_PLATFORM=m
CONFIG_BT=m
CONFIG_BT_RFCOMM=m
CONFIG_BT_RFCOMM_TTY=y
CONFIG_BT_BNEP=m
CONFIG_BT_BNEP_MC_FILTER=y
CONFIG_BT_BNEP_PROTO_FILTER=y
CONFIG_BT_HIDP=m
CONFIG_BT_HCIBTUSB=m
CONFIG_BT_HCIBTSDIO=m
CONFIG_BT_HCIUART=m
CONFIG_BT_HCIUART_BCSP=y
CONFIG_BT_HCIBCM203X=m
CONFIG_BT_HCIBPA10X=m
CONFIG_BT_HCIBFUSB=m
CONFIG_BT_HCIVHCI=m
CONFIG_BT_MRVL=m
CONFIG_BT_MRVL_SDIO=m
CONFIG_CFG80211=m
CONFIG_MAC80211=m
CONFIG_DEVTMPFS=y
CONFIG_DEVTMPFS_MOUNT=y
CONFIG_OMAP_OCP2SCP=y
CONFIG_CONNECTOR=m
CONFIG_MTD=y
CONFIG_MTD_CMDLINE_PARTS=y
CONFIG_MTD_BLOCK=y
CONFIG_MTD_OOPS=y
CONFIG_MTD_CFI=y
CONFIG_MTD_CFI_INTELEXT=y
CONFIG_MTD_PHYSMAP=y
CONFIG_MTD_PHYSMAP_OF=y
CONFIG_MTD_ONENAND=y
CONFIG_MTD_ONENAND_VERIFY_WRITE=y
CONFIG_MTD_ONENAND_OMAP2=y
CONFIG_MTD_RAW_NAND=y
CONFIG_MTD_NAND_OMAP2=y
CONFIG_MTD_NAND_OMAP_BCH=y
CONFIG_MTD_SPI_NOR=m
CONFIG_MTD_UBI=y
CONFIG_BLK_DEV_LOOP=y
CONFIG_BLK_DEV_RAM=y
CONFIG_BLK_DEV_RAM_SIZE=16384
CONFIG_SRAM=y
CONFIG_EEPROM_AT24=m
CONFIG_EEPROM_93CX6=y
CONFIG_BLK_DEV_SD=y
CONFIG_SCSI_SCAN_ASYNC=y
CONFIG_ATA=y
CONFIG_SATA_AHCI_PLATFORM=y
CONFIG_NETDEVICES=y
CONFIG_BONDING=m
CONFIG_WIREGUARD=m
CONFIG_MACVLAN=m
CONFIG_MACVTAP=m
CONFIG_IPVLAN=m
CONFIG_IPVTAP=m
CONFIG_VXLAN=m
CONFIG_TUN=m
# CONFIG_NET_VENDOR_ALACRITECH is not set
# CONFIG_NET_VENDOR_AMAZON is not set
# CONFIG_NET_VENDOR_AQUANTIA is not set
# CONFIG_NET_VENDOR_ARC is not set
# CONFIG_NET_VENDOR_AURORA is not set
# CONFIG_NET_VENDOR_BROADCOM is not set
# CONFIG_NET_VENDOR_CADENCE is not set
# CONFIG_NET_VENDOR_CAVIUM is not set
# CONFIG_NET_VENDOR_CIRRUS is not set
# CONFIG_NET_VENDOR_CORTINA is not set
# CONFIG_NET_VENDOR_EZCHIP is not set
# CONFIG_NET_VENDOR_FARADAY is not set
# CONFIG_NET_VENDOR_GOOGLE is not set
# CONFIG_NET_VENDOR_HISILICON is not set
# CONFIG_NET_VENDOR_HUAWEI is not set
# CONFIG_NET_VENDOR_INTEL is not set
# CONFIG_NET_VENDOR_MARVELL is not set
# CONFIG_NET_VENDOR_MELLANOX is not set
# CONFIG_NET_VENDOR_MICREL is not set
# CONFIG_NET_VENDOR_MICROCHIP is not set
# CONFIG_NET_VENDOR_MICROSEMI is not set
# CONFIG_NET_VENDOR_NATSEMI is not set
# CONFIG_NET_VENDOR_NETRONOME is not set
# CONFIG_NET_VENDOR_NI is not set
# CONFIG_NET_VENDOR_PENSANDO is not set
# CONFIG_NET_VENDOR_QUALCOMM is not set
# CONFIG_NET_VENDOR_RENESAS is not set
# CONFIG_NET_VENDOR_ROCKER is not set
# CONFIG_NET_VENDOR_SAMSUNG is not set
# CONFIG_NET_VENDOR_SEEQ is not set
# CONFIG_NET_VENDOR_SOLARFLARE is not set
CONFIG_SMC91X=y
CONFIG_SMC911X=y
CONFIG_SMSC911X=y
# CONFIG_NET_VENDOR_SOCIONEXT is not set
# CONFIG_NET_VENDOR_STMICRO is not set
# CONFIG_NET_VENDOR_SYNOPSYS is not set
CONFIG_TI_DAVINCI_EMAC=y
CONFIG_TI_CPSW=y
# CONFIG_NET_VENDOR_VIA is not set
# CONFIG_NET_VENDOR_WIZNET is not set
# CONFIG_NET_VENDOR_XILINX is not set
CONFIG_LED_TRIGGER_PHY=y
CONFIG_MICROCHIP_T1_PHY=y
CONFIG_SMSC_PHY=y
CONFIG_USB_USBNET=m
CONFIG_USB_NET_SMSC75XX=m
CONFIG_USB_NET_SMSC95XX=m
# CONFIG_USB_NET_NET1080 is not set
# CONFIG_USB_NET_CDC_SUBSET is not set
# CONFIG_USB_NET_ZAURUS is not set
# CONFIG_WLAN_VENDOR_ADMTEK is not set
# CONFIG_WLAN_VENDOR_ATH is not set
# CONFIG_WLAN_VENDOR_ATMEL is not set
# CONFIG_WLAN_VENDOR_BROADCOM is not set
# CONFIG_WLAN_VENDOR_CISCO is not set
# CONFIG_WLAN_VENDOR_INTEL is not set
# CONFIG_WLAN_VENDOR_INTERSIL is not set
# CONFIG_WLAN_VENDOR_MARVELL is not set
# CONFIG_WLAN_VENDOR_MEDIATEK is not set
# CONFIG_WLAN_VENDOR_MICROCHIP is not set
# CONFIG_WLAN_VENDOR_RALINK is not set
# CONFIG_WLAN_VENDOR_REALTEK is not set
# CONFIG_WLAN_VENDOR_RSI is not set
# CONFIG_WLAN_VENDOR_ST is not set
# CONFIG_WLAN_VENDOR_TI is not set
# CONFIG_WLAN_VENDOR_ZYDAS is not set
# CONFIG_WLAN_VENDOR_QUANTENNA is not set
CONFIG_INPUT_LEDS=m
CONFIG_INPUT_POLLDEV=m
CONFIG_INPUT_EVDEV=m
CONFIG_KEYBOARD_ATKBD=m
CONFIG_KEYBOARD_GPIO=m
CONFIG_KEYBOARD_MATRIX=m
CONFIG_KEYBOARD_OMAP4=m
CONFIG_KEYBOARD_TWL4030=m
# CONFIG_INPUT_MOUSE is not set
CONFIG_INPUT_TOUCHSCREEN=y
CONFIG_TOUCHSCREEN_ADS7846=m
CONFIG_TOUCHSCREEN_EDT_FT5X06=m
CONFIG_TOUCHSCREEN_TI_AM335X_TSC=m
CONFIG_TOUCHSCREEN_PIXCIR=m
CONFIG_TOUCHSCREEN_TSC2005=m
CONFIG_TOUCHSCREEN_TSC2007=m
CONFIG_INPUT_MISC=y
CONFIG_INPUT_TPS65218_PWRBUTTON=m
CONFIG_INPUT_TWL4030_PWRBUTTON=m
CONFIG_INPUT_PALMAS_PWRBUTTON=m
CONFIG_SERIO=m
CONFIG_VT_HW_CONSOLE_BINDING=y
# CONFIG_LEGACY_PTYS is not set
CONFIG_SERIAL_8250=y
CONFIG_SERIAL_8250_CONSOLE=y
CONFIG_SERIAL_8250_NR_UARTS=32
CONFIG_SERIAL_8250_EXTENDED=y
CONFIG_SERIAL_8250_MANY_PORTS=y
CONFIG_SERIAL_8250_SHARE_IRQ=y
CONFIG_SERIAL_8250_DETECT_IRQ=y
CONFIG_SERIAL_8250_RSA=y
CONFIG_SERIAL_8250_OMAP=y
CONFIG_SERIAL_OF_PLATFORM=y
CONFIG_SERIAL_OMAP=y
CONFIG_SERIAL_OMAP_CONSOLE=y
CONFIG_HW_RANDOM=y
CONFIG_I2C_CHARDEV=y
CONFIG_SPI=y
CONFIG_SPI_OMAP24XX=y
CONFIG_SPI_TI_QSPI=m
CONFIG_SPI_SPIDEV=m
CONFIG_HSI=m
CONFIG_OMAP_SSI=m
CONFIG_PINCTRL_SINGLE=y
CONFIG_DEBUG_GPIO=y
CONFIG_GPIO_SYSFS=y
CONFIG_GPIO_PCA953X=m
CONFIG_GPIO_PCF857X=y
CONFIG_GPIO_PALMAS=y
CONFIG_GPIO_TWL4030=y
CONFIG_POWER_RESET=y
CONFIG_BATTERY_BQ27XXX=m
CONFIG_CHARGER_ISP1704=m
CONFIG_CHARGER_TWL4030=m
CONFIG_CHARGER_BQ2415X=m
CONFIG_CHARGER_BQ24190=m
CONFIG_CHARGER_BQ24735=m
CONFIG_SENSORS_GPIO_FAN=m
CONFIG_SENSORS_LM75=m
CONFIG_SENSORS_TMP102=m
CONFIG_THERMAL_GOV_FAIR_SHARE=y
CONFIG_THERMAL_GOV_USER_SPACE=y
CONFIG_CPU_THERMAL=y
CONFIG_TI_SOC_THERMAL=m
CONFIG_TI_THERMAL=y
CONFIG_OMAP3_THERMAL=y
CONFIG_OMAP4_THERMAL=y
CONFIG_OMAP5_THERMAL=y
CONFIG_DRA752_THERMAL=y
CONFIG_WATCHDOG=y
CONFIG_WATCHDOG_NOWAYOUT=y
CONFIG_OMAP_WATCHDOG=y
CONFIG_TWL4030_WATCHDOG=y
CONFIG_MFD_TI_AM335X_TSCADC=m
CONFIG_MFD_PALMAS=y
CONFIG_MFD_TPS65217=y
CONFIG_MFD_TPS65218=y
CONFIG_MFD_TPS65910=y
CONFIG_MFD_TWL4030_AUDIO=y
CONFIG_TWL6040_CORE=y
CONFIG_REGULATOR_PALMAS=y
CONFIG_REGULATOR_PBIAS=y
CONFIG_REGULATOR_TI_ABB=y
CONFIG_REGULATOR_TPS62360=m
CONFIG_REGULATOR_TPS65023=y
CONFIG_REGULATOR_TPS6507X=y
CONFIG_REGULATOR_TPS65217=y
CONFIG_REGULATOR_TPS65218=y
CONFIG_REGULATOR_TPS65910=y
CONFIG_REGULATOR_TWL4030=y
CONFIG_HID_GENERIC=m
CONFIG_USB_HIDDEV=y
CONFIG_USB_KBD=m
CONFIG_USB_MOUSE=m
CONFIG_USB=m
CONFIG_USB_ANNOUNCE_NEW_DEVICES=y
CONFIG_USB_MON=m
CONFIG_USB_XHCI_HCD=m
CONFIG_USB_EHCI_HCD=m
CONFIG_USB_OHCI_HCD=m
CONFIG_USB_WDM=m
CONFIG_USB_STORAGE=m
CONFIG_USB_MUSB_HDRC=m
CONFIG_USB_MUSB_DSPS=m
CONFIG_USB_TI_CPPI41_DMA=y
CONFIG_USB_DWC3=m
CONFIG_USB_TEST=m
CONFIG_USB_GADGET=m
CONFIG_USB_GADGET_DEBUG=y
CONFIG_USB_GADGET_DEBUG_FILES=y
CONFIG_USB_CONFIGFS=m
CONFIG_USB_CONFIGFS_SERIAL=y
CONFIG_USB_CONFIGFS_ACM=y
CONFIG_USB_CONFIGFS_OBEX=y
CONFIG_USB_CONFIGFS_NCM=y
CONFIG_USB_CONFIGFS_ECM=y
CONFIG_USB_CONFIGFS_ECM_SUBSET=y
CONFIG_USB_CONFIGFS_RNDIS=y
CONFIG_USB_CONFIGFS_EEM=y
CONFIG_USB_CONFIGFS_MASS_STORAGE=y
CONFIG_USB_CONFIGFS_F_LB_SS=y
CONFIG_USB_CONFIGFS_F_FS=y
CONFIG_USB_CONFIGFS_F_HID=y
CONFIG_USB_ZERO=m
CONFIG_MMC=y
CONFIG_SDIO_UART=y
CONFIG_MMC_SDHCI=y
CONFIG_MMC_SDHCI_PLTFM=y
CONFIG_MMC_OMAP=y
CONFIG_MMC_OMAP_HS=y
CONFIG_MMC_SDHCI_OMAP=y
CONFIG_NEW_LEDS=y
CONFIG_LEDS_CLASS=y
CONFIG_LEDS_GPIO=y
CONFIG_LEDS_PWM=y
CONFIG_LEDS_TRIGGERS=y
CONFIG_LEDS_TRIGGER_TIMER=y
CONFIG_LEDS_TRIGGER_ONESHOT=y
CONFIG_LEDS_TRIGGER_HEARTBEAT=y
CONFIG_LEDS_TRIGGER_BACKLIGHT=m
CONFIG_LEDS_TRIGGER_CPU=y
CONFIG_LEDS_TRIGGER_GPIO=y
CONFIG_LEDS_TRIGGER_DEFAULT_ON=y
CONFIG_LEDS_TRIGGER_TRANSIENT=y
CONFIG_RTC_CLASS=y
CONFIG_RTC_DRV_DS1307=m
CONFIG_RTC_DRV_TWL92330=y
CONFIG_RTC_DRV_TWL4030=m
CONFIG_RTC_DRV_PALMAS=m
CONFIG_RTC_DRV_OMAP=y
CONFIG_DMADEVICES=y
CONFIG_UIO=m
CONFIG_UIO_PRUSS=m
CONFIG_COMMON_CLK_PALMAS=m
CONFIG_HWSPINLOCK=y
CONFIG_HWSPINLOCK_OMAP=m
CONFIG_MAILBOX=y
CONFIG_OMAP2PLUS_MBOX=m
# CONFIG_IOMMU_SUPPORT is not set
CONFIG_REMOTEPROC=y
CONFIG_WKUP_M3_RPROC=m
CONFIG_SOC_TI=y
CONFIG_WKUP_M3_IPC=m
CONFIG_TI_PRUSS=m
CONFIG_TI_EMIF=m
CONFIG_IIO=m
CONFIG_TI_AM335X_ADC=m
CONFIG_PWM=y
CONFIG_PWM_OMAP_DMTIMER=m
CONFIG_PWM_TIECAP=m
CONFIG_PWM_TIEHRPWM=m
CONFIG_PWM_TWL=m
CONFIG_PWM_TWL_LED=m
CONFIG_TI_PRUSS_INTC=m
CONFIG_PHY_DM816X_USB=m
CONFIG_OMAP_USB2=m
CONFIG_TI_PIPE3=y
CONFIG_EXT2_FS=y
CONFIG_EXT3_FS=y
CONFIG_FANOTIFY=y
CONFIG_QUOTA=y
CONFIG_QFMT_V2=y
CONFIG_AUTOFS4_FS=m
CONFIG_OVERLAY_FS=y
CONFIG_MSDOS_FS=y
CONFIG_VFAT_FS=y
CONFIG_TMPFS=y
CONFIG_TMPFS_POSIX_ACL=y
CONFIG_CONFIGFS_FS=y
CONFIG_JFFS2_FS=y
CONFIG_JFFS2_SUMMARY=y
CONFIG_JFFS2_FS_XATTR=y
CONFIG_JFFS2_COMPRESSION_OPTIONS=y
CONFIG_JFFS2_LZO=y
CONFIG_JFFS2_RUBIN=y
CONFIG_UBIFS_FS=y
CONFIG_NFS_FS=y
CONFIG_NFS_V3_ACL=y
CONFIG_NFS_V4=y
CONFIG_ROOT_NFS=y
CONFIG_NLS_CODEPAGE_437=y
CONFIG_NLS_ISO8859_1=y
CONFIG_SECURITY=y
CONFIG_CRYPTO_DH=m
CONFIG_CRYPTO_ECRDSA=m
CONFIG_CRYPTO_CURVE25519=m
CONFIG_CRYPTO_CHACHA20POLY1305=m
CONFIG_CRYPTO_AEGIS128=m
CONFIG_CRYPTO_SEQIV=m
CONFIG_CRYPTO_ECHAINIV=m
CONFIG_CRYPTO_CTS=m
CONFIG_CRYPTO_PCBC=m
CONFIG_CRYPTO_CRC32=m
CONFIG_CRYPTO_MICHAEL_MIC=y
CONFIG_CRYPTO_AES_TI=m
CONFIG_CRYPTO_BLOWFISH=m
CONFIG_CRYPTO_DES=m
CONFIG_CRYPTO_FCRYPT=m
CONFIG_CRYPTO_LZ4=m
CONFIG_CRYPTO_DEV_OMAP=m
CONFIG_CRYPTO_DEV_OMAP_SHAM=m
CONFIG_CRYPTO_DEV_OMAP_AES=m
CONFIG_CRYPTO_DEV_OMAP_DES=m
CONFIG_CRC_CCITT=y
CONFIG_CRC_T10DIF=y
CONFIG_CRC_ITU_T=y
CONFIG_CRC7=y
CONFIG_LIBCRC32C=y
CONFIG_DMA_CMA=y
CONFIG_PRINTK_TIME=y
# CONFIG_DEBUG_BUGVERBOSE is not set
CONFIG_DEBUG_INFO=y
CONFIG_MAGIC_SYSRQ=y
CONFIG_SCHEDSTATS=y
CONFIG_PROVE_LOCKING=y

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Thomas:

    适用于 AM335x 的最新处理器 SDK 为 v8.2.0.24。 您是否看到此 SDK 版本存在相同的问题?

    我还没有在 AM335x 上验证内核 v8.4.1.2。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我将尝试8.2.0.24 -谢谢。

    与此同时,我也在 dmesg 看到了这一点。 我没有使用 PRU、因此 我尝试使用 DTS 中的以下更改来禁用它。   

    dmesg:

    [   22.902113] remoteproc remoteproc0: wkup_m3 is available
    [   23.597782] wkup_m3_ipc 44e11324.wkup_m3_ipc: IPC Request for A8->M3 Channel failed! -517
    [   23.799467] wkup_m3_ipc 44e11324.wkup_m3_ipc: IPC Request for A8->M3 Channel failed! -517
    [   23.865275] usbcore: registered new interface driver usbfs
    [   23.866531] usbcore: registered new interface driver hub
    [   23.866871] usbcore: registered new device driver usb
    [   24.569959] wkup_m3_ipc 44e11324.wkup_m3_ipc: IPC Request for A8->M3 Channel failed! -517
    [   24.616634] wkup_m3_ipc 44e11324.wkup_m3_ipc: IPC Request for A8->M3 Channel failed! -517
    [   24.818250] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
    [   24.865438] remoteproc remoteproc0: powering up wkup_m3
    [   24.867120] remoteproc remoteproc0: Direct firmware load for am335x-pm-firmware.elf failed with error -2
    [   24.867882] remoteproc remoteproc0: request_firmware failed: -2
    [   24.867919] wkup_m3_ipc 44e11324.wkup_m3_ipc: rproc_boot failed

    DTS 更改:

    &mailbox {
      status = "disabled";
    };
    
    &wkup_m3 {
      status = "disabled";
    };
    
    &wkup_m3_ipc {
      status = "disabled";
    };
    

    我已经重新启动了几次、当我仍然看到"OMAP_INTC_Handle_IRQ:伪 IRQ!" 更改 DTS 后,我尚未看到“可疑 RCU 使用情况”错误。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

     在 https://git.ti.com/cgit/ti-linux-kernel/ti-linux-kernel/refs/ 上、我没有看到 8.4.1.2的标签- 我看到的最接近的是  08.02.00.006。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您在第一个帖子中提到了8.4.1.2 (08.04.01.002)。 我没有检查它是否是有效的标签。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    抱歉-是 08.04.01.002 、这是我测试的内容。 我想说的是、我找不到任何名为 08.02.00.024的标签、但确实有  08.02.00.006

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    08.02.00.024是 AM335x 的处理器 SDK 版本、它使用内核标签08.02.00.006。 很抱歉造成混淆。

    https://www.ti.com/tool/download/PROCESSOR-SDK-LINUX-AM335X/08.02.00.24

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    构建自标签 8.2.0.6后 、不会显示"Suspicious RCU usage"(可疑 RCU 使用)消息。  感谢您的帮助!

    需要注意的是、我仍然看到这一点: 它看起来是随机的、至少与任何硬件交互无关。  在启动后的某个时间点、我只会看到它一次。  我应该担心吗?

    [   82.753279] omap_intc_handle_irq: spurious irq!

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Thomas:

    如果不知道详细信息、我认为很难说出是否可以忽略虚假的 IRQ 消息。

    我建议您继续处理您的项目并留意此消息、并测试项目中所需的所有功能、以查看是否一切正常。