您好、TI 专家!
SDK8.4在 SR1.1器件上成功引导、但在 SR1.0上引导失败。
这块板是我们自己的设计、 您能给我一些建议吗?
以下是 SPL 的运行日志。
U-Boot SPL 2021.01 (Dec 28 2022 - 13:48:30 +0800) Model: Texas Instruments K3 J721E SoC SYSFW ABI: 3.1 (firmware rev 0x0008 '8.4.1--v08.04.01 (Jolly Jellyfi') Trying to boot from MMC2 Starting ATF on ARM64 core... NOTICE: BL31: v2.6(release):v2.7-rc0-dirty NOTICE: BL31: Built : 09:18:58, Aug 30 2022 I/TC: I/TC: OP-TEE version: 3.17.0-125-g15a746d28 (gcc version 9.2.1 20191025 (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10))) #1 Tue Aug 30 09:19:19 UTC 2022 aarch64 I/TC: WARNING: This OP-TEE configuration might be insecure! I/TC: WARNING: Please check optee.readthedocs.io/.../porting_guidelines.html I/TC: Primary CPU initializing I/TC: SYSFW ABI: 3.1 (firmware rev 0x0008 '8.4.1--v08.04.01 (Jolly Jellyfi') I/TC: HUK Initialized I/TC: Activated SA2UL device I/TC: Enabled firewalls for SA2UL TRNG device I/TC: SA2UL TRNG initialized I/TC: SA2UL Drivers initialized I/TC: Primary CPU switching to normal world boot U-Boot SPL 2021.01 (Dec 28 2022 - 13:48:17 +0800) Model: Texas Instruments K3 J721E SoC SYSFW ABI: 3.1 (firmware rev 0x0008 '8.4.1--v08.04.01 (Jolly Jellyfi') Trying to boot from MMC2 U-Boot 2021.01 (Dec 28 2022 - 13:48:17 +0800) SoC: J721E SR1.0 GP Model: Texas Instruments K3 J721E SoC DRAM: 4 GiB Flash: 0 Bytes MMC: sdhci@4f80000: 0, sdhci@4fb0000: 1 Loading Environment from FAT... OK In: serial@2800000 Out: serial@2800000 Err: serial@2800000 Net: No ethernet found. Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc1 is current device SD/MMC found on device 1 Failed to load 'boot.scr' 443 bytes read in 10 ms (43 KiB/s) Loaded env from uEnv.txt Importing environment from mmc1 ... Running uenvcmd ... 1 bytes read in 13 ms (0 Bytes/s) Already setup. k3_r5f_rproc r5f@41000000: Core 1 is already in use. No rproc commands work k3_r5f_rproc r5f@41400000: Core 2 is already in use. No rproc commands work 847284 bytes read in 47 ms (17.2 MiB/s) Load Remote Processor 2 with data@addr=0x82000000 847284 bytes: Success! 302028 bytes read in 24 ms (12 MiB/s) Load Remote Processor 3 with data@addr=0x82000000 302028 bytes: Success! Failed to load '/lib/firmware/j7-main-r5f1_0-fw' Failed to load '/lib/firmware/j7-main-r5f1_1-fw' 1473300 bytes read in 72 ms (19.5 MiB/s) Load Remote Processor 6 with data@addr=0x82000000 1473300 bytes: Success! 1473300 bytes read in 72 ms (19.5 MiB/s) Load Remote Processor 7 with data@addr=0x82000000 1473300 bytes: Success! 12980176 bytes read in 547 ms (22.6 MiB/s) Load Remote Processor 8 with data@addr=0x82000000 12980176 bytes: Success! 18520576 bytes read in 775 ms (22.8 MiB/s) 117806 bytes read in 16 ms (7 MiB/s) ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Device Tree to 000000008fee0000, end 000000008fffffff ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x411fd080] [ 0.000000] Linux version 5.10.120-g95b90aa828 (fuquanfeng@RD15) (aarch64-none-linux-gnu-gcc (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 9.2.1 20191025, GNU ld (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 2.33.1.20191209) #1 SMP PREEMPT Fri Dec 30 15:15:30 CST 2022 [ 0.000000] Machine model: Texas Instruments K3 J721E SoC [ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '') [ 0.000000] printk: bootconsole [ns16550a0] enabled [ 0.000000] efi: UEFI not found. [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a0000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a0100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a1000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a1100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a2000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 31 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a2100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a4000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4100000, size 31 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a4100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a6000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a6000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a6100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a6100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a7000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a7000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a7100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a7100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a8000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-c66-dma-memory@a8000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a8100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-c66-memory@a8100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a9000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-c66-dma-memory@a9000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a9100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-c66-memory@a9100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000aa000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-c71-dma-memory@aa000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000aa100000, size 79 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-c71-memory@aa100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000b2000000, size 96 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-dma-memory@b2000000, compatible id shared-dma-pool [ 0.000000] OF: reserved mem: initialized node vision_apps_shared-memories, compatible id dma-heap-carveout [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000d8000000, size 192 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-core-heap-memory-lo@d8000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000e4000000, size 8 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-virtual-eth-queues@e4000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000e4800000, size 24 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-virtual-eth-buffers@e4800000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x0000000880000000, size 624 MiB [ 0.000000] OF: reserved mem: initialized node vision-apps-core-heap-memory-hi@880000000, compatible id shared-dma-pool [ 0.000000] Zone ranges: [ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff] [ 0.000000] DMA32 empty [ 0.000000] Normal [mem 0x0000000100000000-0x00000008ffffffff] [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000080000000-0x000000009e7fffff] [ 0.000000] node 0: [mem 0x000000009e800000-0x00000000aeffffff] [ 0.000000] node 0: [mem 0x00000000af000000-0x00000000afffffff] [ 0.000000] node 0: [mem 0x00000000b0000000-0x00000000b7ffffff] [ 0.000000] node 0: [mem 0x00000000b8000000-0x00000000d7ffffff] [ 0.000000] node 0: [mem 0x00000000d8000000-0x00000000e5ffffff] [ 0.000000] node 0: [mem 0x00000000e6000000-0x00000000ffffffff] [ 0.000000] node 0: [mem 0x0000000880000000-0x00000008a6ffffff] [ 0.000000] node 0: [mem 0x00000008a7000000-0x00000008ffffffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000008ffffffff] [ 0.000000] cma: Reserved 400 MiB at 0x00000000e7000000 [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: Trusted OS migration not required [ 0.000000] psci: SMC Calling Convention v1.2 [ 0.000000] percpu: Embedded 22 pages/cpu s50008 r8192 d31912 u90112 [ 0.000000] Detected PIPT I-cache on CPU0 [ 0.000000] CPU features: detected: GIC system register CPU interface [ 0.000000] CPU features: detected: EL2 vector hardening [ 0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923 [ 0.000000] CPU features: detected: Spectre-BHB [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1032192 [ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=47040000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),256k(ospi.env),1m(ospi.sysfw),256k(ospi.env.backup),57088k@8m(ospi.rootfs),256k(ospi.phypattern);47034000.hyperbus:512k(hbmc.tiboot3),2m(hbmc.tispl),4m(hbmc.u-boot),256k(hbmc.env),1m(hbmc.sysfw),-@8m(hbmc.rootfs) root=PARTUUID=6623acc4-02 rw rootfstype=ext4 rootwait [ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear) [ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] software IO TLB: mapped [mem 0x000000009a800000-0x000000009e800000] (64MB) [ 0.000000] Memory: 1827988K/4194304K available (10880K kernel code, 1126K rwdata, 4188K rodata, 1792K init, 431K bss, 1956716K reserved, 409600K cma-reserved) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] rcu: RCU event tracing is enabled. [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2. [ 0.000000] Trampoline variant of Tasks RCU enabled. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies. [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2 [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode [ 0.000000] GICv3: 960 SPIs implemented [ 0.000000] GICv3: 0 Extended SPIs implemented [ 0.000000] GICv3: Distributor has no Range Selector support [ 0.000000] GICv3: 16 PPIs implemented [ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001900000 [ 0.000000] ITS [mem 0x01820000-0x0182ffff] [ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS [ 0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19 [ 0.000000] ITS@0x0000000001820000: allocated 524288 Devices @8a7800000 (flat, esz 8, psz 64K, shr 0) [ 0.000000] ITS: using cache flushing for cmd queue [ 0.000000] GICv3: using LPI property table @0x00000008a7030000 [ 0.000000] GIC: using cache flushing for LPI property table [ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x00000008a7040000 [ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns [ 0.000001] sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns [ 0.008409] Console: colour dummy device 80x25 [ 0.012974] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000) [ 0.023644] pid_max: default: 32768 minimum: 301 [ 0.028400] LSM: Security Framework initializing [ 0.033158] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear) [ 0.040736] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear) [ 0.049522] rcu: Hierarchical SRCU implementation. [ 0.054579] Platform MSI: msi-controller@1820000 domain created [ 0.060836] PCI/MSI: /bus@100000/interrupt-controller@1800000/msi-controller@1820000 domain created [ 0.070139] EFI services will not be available. [ 0.074872] smp: Bringing up secondary CPUs ... I/TC: Secondary CPU 1 initializing I/TC: Secondary CPU 1 switching to normal world boot [ 0.088145] Detected PIPT I-cache on CPU1 [ 0.088168] GICv3: CPU1: found redistributor 1 region 0:0x0000000001920000 [ 0.088179] GICv3: CPU1: using allocated LPI pending table @0x00000008a7050000 [ 0.088215] CPU1: Booted secondary processor 0x0000000001 [0x411fd080] [ 0.088264] smp: Brought up 1 node, 2 CPUs [ 0.117609] SMP: Total of 2 processors activated. [ 0.122414] CPU features: detected: 32-bit EL0 Support [ 0.127668] CPU features: detected: CRC32 instructions [ 0.141648] CPU: All CPU(s) started at EL2 [ 0.145846] alternatives: patching kernel code [ 0.150873] devtmpfs: initialized [ 0.160084] KASLR disabled due to lack of seed [ 0.164733] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.174695] futex hash table entries: 512 (order: 3, 32768 bytes, linear) [ 0.186837] pinctrl core: initialized pinctrl subsystem [ 0.192492] DMI not present or invalid. [ 0.196739] NET: Registered protocol family 16 [ 0.201965] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations [ 0.209282] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations [ 0.217344] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations [ 0.225645] thermal_sys: Registered thermal governor 'step_wise' [ 0.225647] thermal_sys: Registered thermal governor 'power_allocator' [ 0.232239] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. [ 0.245872] ASID allocator initialised with 65536 entries [ 0.263519] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages [ 0.270374] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages [ 0.277224] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages [ 0.284071] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages [ 0.291534] cryptd: max_cpu_qlen set to 1000 [ 0.297526] k3-chipinfo 43000014.chipid: Family:J721E rev:SR1.0 JTAGID[0x0bb6402f] Detected [ 0.306305] vsys_3v3: supplied by evm_12v0 [ 0.310666] vsys_5v0: supplied by evm_12v0 [ 0.315054] vdd_mmc1: supplied by vsys_3v3 [ 0.319713] iommu: Default domain type: Translated [ 0.324850] SCSI subsystem initialized [ 0.328895] mc: Linux media interface: v0.10 [ 0.333278] videodev: Linux video capture interface: v2.00 [ 0.338907] pps_core: LinuxPPS API ver. 1 registered [ 0.343978] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 0.353316] PTP clock support registered [ 0.357334] EDAC MC: Ver: 3.0.0 [ 0.361076] FPGA manager framework [ 0.364586] Advanced Linux Sound Architecture Driver Initialized. [ 0.371193] clocksource: Switched to clocksource arch_sys_counter [ 0.377516] VFS: Disk quotas dquot_6.6.0 [ 0.381549] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes) [ 0.391190] Carveout Heap: Exported 512 MiB at 0x00000000b8000000 [ 0.397481] NET: Registered protocol family 2 [ 0.402222] IP idents hash table entries: 65536 (order: 7, 524288 bytes, linear) [ 0.410876] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes, linear) [ 0.419631] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear) [ 0.427833] TCP bind hash table entries: 32768 (order: 7, 524288 bytes, linear) [ 0.435642] TCP: Hash tables configured (established 32768 bind 32768) [ 0.442431] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear) [ 0.449324] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear) [ 0.456724] NET: Registered protocol family 1 [ 0.461451] RPC: Registered named UNIX socket transport module. [ 0.467509] RPC: Registered udp transport module. [ 0.472324] RPC: Registered tcp transport module. [ 0.477128] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.483712] PCI: CLS 0 bytes, default 64 [ 0.488091] hw perfevents: enabled with armv8_cortex_a72 PMU driver, 7 counters available [ 0.498425] Initialise system trusted keyrings [ 0.503067] workingset: timestamp_bits=46 max_order=20 bucket_order=0 [ 0.511244] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.517462] NFS: Registering the id_resolver key type [ 0.522648] Key type id_resolver registered [ 0.526922] Key type id_legacy registered [ 0.531046] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 0.537894] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering... [ 0.545535] 9p: Installing v9fs 9p2000 file system support [ 0.570832] Key type asymmetric registered [ 0.575018] Asymmetric key parser 'x509' registered [ 0.580015] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243) [ 0.587574] io scheduler mq-deadline registered [ 0.592198] io scheduler kyber registered [ 0.597547] pinctrl-single 4301c000.pinctrl: 94 pins, size 376 [ 0.603716] pinctrl-single 11c000.pinctrl: 173 pins, size 692 [ 0.611928] k3-ringacc 2b800000.ringacc: Failed to get MSI domain [ 0.618194] k3-ringacc 3c000000.ringacc: Failed to get MSI domain [ 0.625941] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled [ 0.633910] arm-smmu-v3 36600000.iommu: ias 48-bit, oas 48-bit (features 0x00001faf) [ 0.642163] arm-smmu-v3 36600000.iommu: allocated 65536 entries for cmdq [ 0.649245] arm-smmu-v3 36600000.iommu: allocated 32768 entries for evtq [ 0.657877] arm-smmu-v3 36600000.iommu: msi_domain absent - falling back to wired irqs [ 0.670402] brd: module loaded [ 0.676927] loop: module loaded [ 0.680726] megasas: 07.714.04.00-rc1 [ 0.686093] tun: Universal TUN/TAP device driver, 1.6 [ 0.691516] igbvf: Intel(R) Gigabit Virtual Function Network Driver [ 0.697921] igbvf: Copyright (c) 2009 - 2012 Intel Corporation. [ 0.703992] sky2: driver version 1.30 [ 0.708231] VFIO - User Level meta-driver version: 0.3 [ 0.713946] i2c /dev entries driver [ 0.718116] sdhci: Secure Digital Host Controller Interface driver [ 0.724441] sdhci: Copyright(c) Pierre Ossman [ 0.729047] sdhci-pltfm: SDHCI platform and OF driver helper [ 0.735284] ledtrig-cpu: registered to indicate activity on CPUs [ 0.741592] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping .... [ 0.748745] optee: probing for conduit method. [ 0.753306] optee: revision 3.17 (15a746d2) [ 0.753433] optee: dynamic shared memory is enabled E/TC:1 0 std_entry_with_parg:234 Bad arg address 0x8a8074000 [ 0.768234] optee: initialized driver [ 0.772951] NET: Registered protocol family 17 [ 0.777566] 9pnet: Installing 9P2000 support [ 0.781962] Key type dns_resolver registered [ 0.786411] Loading compiled-in X.509 certificates [ 0.795808] k3-ringacc 2b800000.ringacc: Failed to get MSI domain [ 0.802144] k3-ringacc 3c000000.ringacc: Failed to get MSI domain [ 0.809904] ti-sci 44083000.dmsc: ABI: 3.1 (firmware rev 0x0008 '8.4.1--v08.04.01 (Jolly Jellyfi') [ 0.854953] omap_i2c 2010000.i2c: bus 0 rev0.12 at 400 kHz [ 0.861030] omap_i2c 2030000.i2c: bus 1 rev0.12 at 400 kHz [ 0.867444] ti-sci-intr bus@100000:bus@28380000:interrupt-controller2: Interrupt Router 137 domain created [ 0.877420] ti-sci-intr bus@100000:interrupt-controller0: Interrupt Router 131 domain created [ 0.886238] ti-sci-intr bus@100000:main-navss:interrupt-controller1: Interrupt Router 213 domain created [ 0.896112] ti-sci-inta 33d00000.interrupt-controller: Interrupt Aggregator domain 209 created [ 0.905638] k3-ringacc 2b800000.ringacc: Ring Accelerator probed rings:286, gp-rings[96,20] sci-dev-id:235 [ 0.915518] k3-ringacc 2b800000.ringacc: dma-ring-reset-quirk: disabled [ 0.922277] k3-ringacc 2b800000.ringacc: RA Proxy rev. 66346100, num_proxies:64 [ 0.931357] k3-ringacc 3c000000.ringacc: Ring Accelerator probed rings:1024, gp-rings[440,150] sci-dev-id:211 [ 0.941515] k3-ringacc 3c000000.ringacc: dma-ring-reset-quirk: disabled [ 0.948278] k3-ringacc 3c000000.ringacc: RA Proxy rev. 66346100, num_proxies:64 [ 0.956220] printk: console [ttyS2] disabled [ 0.960614] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 21, base_baud = 3000000) is a 8250 [ 0.969356] printk: console [ttyS2] enabled [ 0.969356] printk: console [ttyS2] enabled [ 0.977791] printk: bootconsole [ns16550a0] disabled [ 0.977791] printk: bootconsole [ns16550a0] disabled [ 0.989717] davinci_mdio 46000f00.mdio: Configuring MDIO in manual mode [ 1.035202] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000 [ 1.043544] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver unknown [ 1.051582] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00101, cpsw version 0x6BA80100 Ports: 2 quirks:00000000 [ 1.065564] am65-cpts 310d0000.cpts: CPTS ver 0x4e8a010a, freq:200000000, add_val:4 pps:0
提前感谢。