请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:DRV5057 您好!
我使用 DRV5057进行位置感测。 它工作正常、
但当没有磁体时、它会提供其输出的50%占空比。
我的要求是、我希望输出占空比为0至100%、这会随着 磁体各自的运动呈线性变化。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.