This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TIDA-00122:UCD 8220和 MSP430设计问题

Guru**** 671890 points
Other Parts Discussed in Thread: TIDA-00122
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/simulation-hardware-system-design-tools-group/sim-hw-system-design/f/simulation-hardware-system-design-tools-forum/710272/tida-00122-ucd-8220-and-msp430-design-question

器件型号:TIDA-00122

尊敬的先生:

我的客户需要将直流电压12v 转换为交流电压 AC110V_TOTAL WATTS 100W~150W (60Hz 正弦波)逆变器应用。 有关 TIDA-00122的参考设计、我可以提出几个问题吗?

1.您有 MSP430G2330源代码吗? TIDA-00122参考设计。

2.您是否有变压器(t1_EI33 12引脚 Bobin)的数据表?

如果将输入电压从12v 更改为24V、我需要更改哪些组件或参数?