主题中讨论的其他器件:CC1200
大家好、
我尝试将 CC1200EM 连接到 STM 微控制器、很难访问 CC1200寄存器、另一个线程建议在 cc1200EM 上连接复位和 VDD、但这没有解决我的问题。 有人可以提供帮助吗?
最棒的
哦
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好、
我尝试将 CC1200EM 连接到 STM 微控制器、很难访问 CC1200寄存器、另一个线程建议在 cc1200EM 上连接复位和 VDD、但这没有解决我的问题。 有人可以提供帮助吗?
最棒的
哦
SPI 连接正确、因为我能够在写入后读取每个寄存器
以下是我用于配置寄存器的函数(从评估板上成功的 TC 中导出的 Smart RF)
void CC1200_init (void)
{
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_IOCFG2、SmartRF_setting_IOCFG2);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_Devel_M、SmartRF_setting_Devel_M);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_MODCFG_DEV_E、SmartRF_setting_MODCFG_DEV_E);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_DCFILT_CFG、SmartRF_setting_DCFILT_CFG);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_PREAM_CFG0、SmartRF_setting_PREAM_CFG0);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_IQIC、SmartRF_setting_IQIC);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_CHAN_BW、SmartRF_setting_CHAN_BW);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_MDMCFG1、SmartRF_setting_MDMCFG1);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_MDMCFG0、SmartRF_setting_MDMCFG0);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_SYMBOL_Rate2、SmartRF_setting_symbol_Rate2);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_symbol_rate1、SmartRF_setting_symbol_rate1);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_SYMBOL_RATE0、SmartRF_setting_symbol_RATE0);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_AGC_REF、SmartRF_setting_AGC_REF);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_AGC_CS_THR、SmartRF_setting_AGC_CS_THR);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_AGC_CFG1、SmartRF_setting_AGC_CFG1);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_AGC_CFG0、SmartRF_setting_AGC_CFG0);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_FIFO_CFG、SmartRF_setting_FIFO_CFG);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_FS_CFG、SmartRF_setting_FS_CFG);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_PKT_CFG2、SmartRF_setting_PKT_CFG2);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_PKT_CFG0、SmartRF_setting_PKT_CFG0);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_PKT_LEN、SmartRF_setting_PKT_LEN);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_IF_Mix_CFG、SmartRF_setting_IF_Mix_CFG);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_FREQOFF_CFG、SmartRF_setting_FREQOFF_CFG);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_MDMCFG2、SmartRF_setting_MDMCFG2);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_FREQ2、SmartRF_setting_FREQ2);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_IF_ADC1、SmartRF_setting_IF_ADC1);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_IF_ADC0、SmartRF_setting_IF_ADC0);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_FS_DIG1、SmartRF_setting_FS_DIG1);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_FS_DIG0、SmartRF_setting_FS_DIG0);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_FS_CAL1、SmartRF_setting_FS_CAL1);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_FS_CAL0、SmartRF_setting_FS_CAL0);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_FS_DIVTWO、SmartRF_setting_FS_DIVTWO);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_FS_DSM0、SmartRF_setting_FS_DSM0);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_FS_DVC0、SmartRF_setting_FS_DVC0);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_FS_PFD、SmartRF_setting_FS_PFD);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_FS_PRE、SmartRF_setting_FS_PRE);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_FS_REG_DIV_CML、SmartRF_setting_FS_REG_DIV_CML);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_FS_SPARE、SmartRF_setting_FS_SPARE);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_FS_VCO0、SmartRF_setting_FS_VCO0);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_XOSC5、SmartRF_setting_XOSC5);
ReadWriteExtendedReg (CC1200_WRITE_BIT、CC1200_XOSC1、SmartRF_setting_XOSC1);
}
下面是保存宏的头文件
/*------------------ *
/*从 SmartRF Studio 导出的寄存器地址*/
#define CC1200_IOCFG3 0x0000 /* GPIO3 IO 引脚配置*
#define CC1200_IOCFG2 0x0001 // GPIO2 IO 引脚配置*/
#define CC1200_IOCFG1 0x0002 /* GPIO1 IO 引脚配置*
#define CC1200_IOCFG0 0x0003 // GPIO0 IO 引脚配置*/
#define CC1200_SYNC3 0x0004 //同步字配置[31:24]*/
#define CC1200_SYNC2 0x0005 //同步字配置[23:16]*/
#define CC1200_SYNC1 0x0006 //同步字配置[15:8]*/
#define CC1200_SYNC0 0x0007 //同步字配置[7:0]*/
#define CC1200_SYNC_CFG1 0x0008 //同步字检测配置寄存器 1 */
#define CC1200_SYNC_CFG0 0x0009 //同步字检测配置寄存器 0 */
#define CC1200_DERAING_M 0x000A //频率偏差配置*/
#define CC1200_MODCFG_DEV_E 0x000B /*调制格式和频率偏差配置 *
#define CC1200_DCFILT_CFG 0x000C //数字直流移除配置*/
#define CC1200_PREAMARE_CFG1 0x000D /*前导码长度配置寄存器 1 */
#define CC1200_PREAMARE_CFG0 0x000E //前导码检测配置寄存器 0 */
#define CC1200_IQIC 0x000F //数字图像通道补偿配置*/
#define CC1200_CHAN_BW 0x0010 //通道滤波器配置*/
#define CC1200_MDMCFG1 0x0011 //常规调制解调器参数配置寄存器 1 */
#define CC1200_MDMCFG0 0x0012 //常规调制解调器参数配置寄存器 0 */
#define CC1200_symbol_Rate2 0x0013 /*符号速率配置指数和尾数[1] *
#define CC1200_symbol_rate1 0x0014 /*符号速率配置尾数[15:8]*/
#define CC1200_symbol_RATE0 0x0015 //符号速率配置尾数[7:0]*/
#define CC1200_AGC_REF 0x0016 // AGC 基准电平配置*/
#define CC1200_AGC_CS_THR 0x0017 //载波检测阈值配置*/
#define CC1200_AGC_GAIN_ADJUST 0x0018 /* RSSI 偏移配置*/
#define CC1200_AGC_CFG3 0x0019 //自动增益控制配置寄存器 3 */
#define CC1200_AGC_CFG2 0x001A //自动增益控制配置寄存器 2 */
#define CC1200_AGC_CFG1 0x001B //自动增益控制配置寄存器 1 */
#define CC1200_AGC_CFG0 0x001C //自动增益控制配置寄存器 0 */
#define CC1200_FIFO_CFG 0x001D /* FIFO 配置*
#define CC1200_DEV_ADDR 0x001E //器件地址配置*/
#define CC1200_Settling _CFG 0x001F /*频率合成器校准和稳定控制 *
#define CC1200_FS_CFG 0x0020 //频率合成器配置*/
#define CC1200_WOR_CFG1 0x0021 // eWOR 配置寄存器 1 */
#define CC1200_WOR_CFG0 0x0022 // eWOR 配置寄存器 0 */
#define CC1200_WOR_EVENT0_MSB 0x0023 //事件0配置 MSB */
#define CC1200_WOR_EVENT0_LSB 0x0024 //事件0配置 LSB */
#define CC1200_RXDCM_TIME 0x0025 // RX 占空比模式配置*/
#define CC1200_PKT_CFG2 0x0026 //数据包配置寄存器 2 */
#define CC1200_PKT_CFG1 0x0027 //数据包配置寄存器 1 */
#define CC1200_PKT_CFG0 0x0028 //数据包配置寄存器 0 */
#define CC1200_RFEND_CFG1 0x0029 // RFEND 配置寄存器 1 */
#define CC1200_RFEND_CFG0 0x002A /* RFEND 配置寄存器 0 */
#define CC1200_PA_CFG1 0x002B //功率放大器配置寄存器 1 */
#define CC1200_PA_CFG0 0x002C /*功率放大器配置寄存器 0 */
#define CC1200_ASK_CFG 0x002D /* ASK 配置*/
#define CC1200_PKT_LEN 0x002E //数据包长度配置*/
#define CC1200_IF_Mix _CFG 0x2F00 /* IF Mix Configuration *
#define CC1200_FREQOFF_CFG 0x2F01 /*频率偏移校正配置*
#define CC1200_TOC_CFG 0x2F02 //定时偏移校正配置*/
#define CC1200_MARC_SPARE 0x2F03 // Marc Spare *
#define CC1200_ECG_CFG 0x2F04 //外部时钟频率配置*/
#define CC1200_MDMCFG2 0x2F05 //常规调制解调器参数配置寄存器 2 */
#define CC1200_EXT_CTRL 0x2F06 /*外部控制配置*/
#define CC1200_RCCAL_Fine 0x2F07 // RC 振荡器校准 Fine */
#define CC1200_RCCAL_ROR 0x2F08 // RC 振荡器校准粗调*/
#define CC1200_RCCAL_OFFSET 0x2F09 // RC 振荡器校准时钟偏移*
#define CC1200_FREQOFF1 0x2F0A /*频率偏移 MSB *
#define CC1200_FREQOFF0 0x2F0B /*频率偏移 LSB *
#define CC1200_FREQ2 0x2F0C /*频率配置[23:16]*/
#define CC1200_FREQ1 0x2F0D /*频率配置[15:8]*/
#define CC1200_FREQ0 0x2F0E /*频率配置[7:0]*
#define CC1200_IF_ADC2 0x2F0F /*模数转换器配置寄存器 2 */
#define CC1200_IF_ADC1 0x2F10 //模数转换器配置寄存器 1 */
#define CC1200_IF_ADC0 0x2F11 /*模数转换器配置寄存器 0 */
#define CC1200_FS_DIG1 0x2F12 //频率合成器数字寄存器 1 */
#define CC1200_FS_DIG0 0x2F13 //频率合成器数字寄存器 0 */
#define CC1200_FS_CAL3 0x2F14 //频率合成器校准寄存器 3 */
#define CC1200_FS_CAL2 0x2F15 //频率合成器校准寄存器 2 */
#define CC1200_FS_CAL1 0x2F16 //频率合成器校准寄存器 1 */
#define CC1200_FS_CAL0 0x2F17 //频率合成器校准寄存器 0 */
#define CC1200_FS_CHP 0x2F18 //频率合成器电荷泵配置*/
#define CC1200_FS_DIVTWO 0x2F19 //频率合成器除以2 */
#define CC1200_FS_DSM1 0x2F1A /* FS 数字合成器模块配置寄存器 1 */
#define CC1200_FS_DSM0 0x2F1B /* FS 数字合成器模块配置寄存器 0 */
#define CC1200_FS_DVC1 0x2F1C /*频率合成器分频器链配置. *
#define CC1200_FS_DVC0 0x2F1D /*频率合成器分频器链配置. *
#define CC1200_FS_LBI 0x2F1E /*频率合成器本地偏置配置*
#define CC1200_FS_PFD 0x2F1F //频率合成器相位频率检测器连接 *
#define CC1200_FS_PRE 0x2F20 //频率合成器预分频器配置*/
#define CC1200_FS_REG_DIV_CML 0x2F21 //频率合成器分频器稳压器配置 *
#define CC1200_FS_SPARE 0x2F22 /*频率合成器备件*
#define CC1200_FS_VCO4 0x2F23 /* FS 压控振荡器配置寄存器 *
#define CC1200_FS_VCO3 0x2F24 /* FS 压控振荡器配置寄存器 *
#define CC1200_FS_VCO2 0x2F25 /* FS 压控振荡器配置寄存器 *
#define CC1200_FS_VCO1 0x2F26 /* FS 压控振荡器配置寄存器 *
#define CC1200_FS_VCO0 0x2F27 /* FS 压控振荡器配置寄存器 *
#define CC1200_GBIAS6 0x2F28 //全局偏置配置寄存器 6 */
#define CC1200_GBIAS5 0x2F29 //全局偏置配置寄存器 5 */
#define CC1200_GBIAS4 0x2F2A /*全局偏置配置寄存器 4 */
#define CC1200_GBIAS3 0x2F2B //全局偏置配置寄存器 3 */
#define CC1200_GBIAS2 0x2F2C /*全局偏置配置寄存器 2 */
#define CC1200_GBIAS1 0x2F2D /*全局偏置配置寄存器 1 */
#define CC1200_GBIAS0 0x2F2E/*全局偏置配置寄存器 0 */
#define CC1200_IFAMP 0x2F2F //中间频率放大器配置*/
#define CC1200_LNA 0x2F30 //低噪声放大器配置*/
#define CC1200_RXMIX 0x2F31 // RX 混频器配置*/
#define CC1200_XOSC5 0x2F32 //晶体振荡器配置寄存器 5 */
#define CC1200_XOSC4 0x2F33 //晶体振荡器配置寄存器 4 */
#define CC1200_XOSC3 0x2F34 //晶体振荡器配置寄存器 3 */
#define CC1200_XOSC2 0x2F35 //晶体振荡器配置寄存器 2 */
#define CC1200_XOSC1 0x2F36 //晶体振荡器配置寄存器 1 */
#define CC1200_XOSC0 0x2F37 //晶体振荡器配置寄存器 0 */
#define CC1200_ANALOG_SPARE 0x2F38 /*模拟备件*
#define CC1200_PA_CFG3 0x2F39 //功率放大器配置寄存器 3 */
#define CC1200_WOR_TIME1 0x2F64 // eWOR 计时器计数器值 MSB */
#define CC1200_WOR_TIME0 0x2F65 // eWOR 计时器计数器值 LSB *
#define CC1200_WOR_CAPTURE1 0x2F66 // eWOR 计时器捕获值 MSB *
#define CC1200_WOR_CAPTURE0 0x2F67 //* eWOR 计时器捕获值 LSB *
#define CC1200_BIST 0x2F68 // Marc 内置自检*/
#define CC1200_DCFILTOFFSET_I1 0x2F69 //直流滤波器偏移 I MSB *
#define CC1200_DCFILTOFFSET_I0 0x2F6A /*直流滤波器偏移 I LSB *
#define CC1200_DCFILTOFFSET_Q1 0x2F6B //直流滤波器偏移 Q MSB *
#define CC1200_DCFILTOFFSET_Q0 0x2F6C /*直流滤波器偏移 Q LSB *
#define CC1200_IQIE_I1 0x2F6D /* IQ 不平衡值 I MSB */
#define CC1200_IQIE_I0 0x2F6E /* IQ 不平衡值 I LSB */
#define CC1200_IQIE_Q1 0x2F6F /* IQ 不平衡值 Q MSB */
#define CC1200_IQIE_Q0 0x2F70 // IQ 不平衡值 Q LSB */
#define CC1200_RSSI1 0x2F71 //接收信号强度指示器寄存器 1 */
#define CC1200_RSSI0 0x2F72 //接收信号强度指示器寄存器0 */
#define CC1200_MARCSTATE 0x2F73 /* MARC 状态*/
#define CC1200_LQI_VAL 0x2F74 //链接质量指示器值*/
#define CC1200_PQT_SYNC_ERR 0x2F75 //前导码和同步字错误*/
#define CC1200_DEM_STATUS 0x2F76 /*解调器状态*
#define CC1200_FREQOFF_EST1 0x2F77 //频率偏移估算 MSB *
#define CC1200_FREQOFF_EST0 0x2F78 //频率偏移估算 LSB *
#define CC1200_AGC_GAIN3 0x2F79 //自动增益控制寄存器 3 */
#define CC1200_AGC_GAIN2 0x2F7A //自动增益控制寄存器 2 */
#define CC1200_AGC_GAIN1 0x2F7B //自动增益控制寄存器 1 */
#define CC1200_AGC_GAIN0 0x2F7C //自动增益控制寄存器 0 */
#define CC1200_CFM_RX_DATA_OUT 0x2F7D //自定义频率调制 RX 数据*/
#define CC1200_CFM_TX_DATA_IN 0x2F7E //自定义频率调制 TX 数据*/
#define CC1200_ASK_SOFT_RX_DATA 0x2F7F /* ASK 软决策输出*/
#define CC1200_RNDGEN 0x2F80 //随机数发生器值*/
#define CC1200_MAGN2 0x2F81 // CORDIC 之后的信号幅度[16]*
#define CC1200_MAGN1 0x2F82 // CORDIC 之后的信号幅度[15:8]*
#define CC1200_MAGN0 0x2F83 // CORDIC 之后的信号幅度[7:0]*/
#define CC1200_ANG1 0x2F84 // CORDIC 后的信号角度[9:8]*
#define CC1200_Ang0 0x2F85 // CORDIC 之后的信号角度[7:0]*/
#define CC1200_CHFILT_I2 0x2F86 /*通道滤波器数据实数部分[16]*/
#define CC1200_CHFILT_I1 0x2F87 //通道滤波器数据实数部分[15:8]*
#define CC1200_CHFILT_I0 0x2F88 //通道滤波器数据实数部分[7:0]*/
#define CC1200_CHFILT_Q2 0x2F89 //通道滤波器数据虚部[16]*/
#define CC1200_CHFILT_Q1 0x2F8A /*通道滤波器数据虚部[15:8]*
#define CC1200_CHFILT_Q0 0x2F8B /*通道滤波器数据虚部[7:0]*
#define CC1200_GPIO_STATUS 0x2F8C //通用输入/输出状态*/
#define CC1200_FSCAL_CTRL 0x2F8D /*频率合成器校准控制*
#define CC1200_PHASE_ADJUST 0x2F8E /*频率合成器相位调整*
#define CC1200_PARTNUMBER 0x2F8F /*器件型号*/
#define CC1200_PARTVERSION 0x2F90 //器件版本*/
#define CC1200_serial_status 0x2F91 //串行状态*
#define CC1200_MODEM_STATUS1 0x2F92 /*调制解调器状态寄存器 1 */
#define CC1200_MODEM_STATUS0 0x2F93 //调制解调器状态寄存器 0 */
#define CC1200_MARC_STATUS1 0x2F94 /* MARC 状态寄存器 1 */
#define CC1200_MARC_STATUS0 0x2F95 // MARC 状态寄存器 0 */
#define CC1200_PA_IFAMP_TEST 0x2F96 //功率放大器中间频率放大器 T. *
#define CC1200_FSRF_TEST 0x2F97 /*频率合成器测试*
#define CC1200_PRE_TEST 0x2F98 /*频率合成器预分频器测试*
#define CC1200_PRE_OVR 0x2F99 //频率合成器预分频器覆盖*/
#define CC1200_ADC_TEST 0x2F9A /*模数转换器测试*
#define CC1200_DVC_TEST 0x2F9B /*数字分频器链测试*
#define CC1200_ATEST 0x2F9C //模拟测试*/
#define CC1200_ATEST_LVDS 0x2F9D /*模拟测试 LVDS *
#define CC1200_ATEST_MODE 0x2F9E //模拟测试模式*/
#define CC1200_XOSC_TEST1 0x2F9F //晶体振荡器测试寄存器 1 */
#define CC1200_XOSC_TEST0 0x2FA0 //晶体振荡器测试寄存器 0 */
#define CC1200_AES 0x2FA1/* AES *
#define CC1200_MDM_TEST 0x2FA2/*调制解调器测试*
#define CC1200_RXFIRST 0x2FD2 /* RX FIFO 指针第一个入口*/
#define CC1200_TXFIRST 0x2FD3 // TX FIFO 指针第一个入口*
#define CC1200_RXLAST 0x2FD4 // RX FIFO 指针最后一个条目*/
#define CC1200_TXLAST 0x2FD5 // TX FIFO 指针最后一个条目*/
#define CC1200_NUM_TXBYTES 0x2FD6 // TX FIFO 状态*/
#define CC1200_NUM_RXBYTES 0x2FD7 // RX FIFO 状态*/
#define CC1200_FIFO_NUM_TXBYTES 0x2FD8 // TX FIFO 状态*/
#define CC1200_FIFO_NUM_RXBYTES 0x2FD9 // RX FIFO 状态*/
#define CC1200_RXFIFO_PRE_BUF 0x2FDA // RX FIFO 状态*/
#define CC1200_AES_KEY15 0x2FE0 //高级加密标准密钥[127:120]*/
#define CC1200_AES_KEY14 0x2FE1/*高级加密标准密钥[119:112]*/
#define CC1200_AES_KEY13 0x2FE2/*高级加密标准密钥[111:104]*/
#define CC1200_AES_KEY12 0x2FE3 //高级加密标准密钥[103:96]*/
#define CC1200_AES_KEY11 0x2FE4 //高级加密标准密钥[95:88]*/
#define CC1200_AES_KEY10 0x2FE5 //高级加密标准密钥[87:80]*/
#define CC1200_AES_KEY9 0x2FE6 //高级加密标准密钥[79:72]*/
#define CC1200_AES_KEY8 0x2FE7 //高级加密标准密钥[71:64]*/
#define CC1200_AES_KEY7 0x2FE8 //高级加密标准密钥[63:56]*/
#define CC1200_AES_KEY6 0x2FE9 //高级加密标准密钥[55:48]*/
#define CC1200_AES_KEY5 0x2FEA/*高级加密标准密钥[47:40]*/
#define CC1200_AES_KEY4 0x2FEB/*高级加密标准密钥[39:32]*/
#define CC1200_AES_key3 0x2FEC //高级加密标准密钥[31:24]*/
#define CC1200_AES_key2 0x2FED //高级加密标准密钥[23:16]*/
#define CC1200_AES_key1 0x2FEE //高级加密标准密钥[15:8]*/
#define CC1200_AES_KEY0 0x2FEF/*高级加密标准密钥[7:0]*/
#define CC1200_AES_BUFFER15 0x2FF0 /*高级加密标准缓冲器[127:120]*/
#define CC1200_AES_BUFFER14 0x2FF1 /*高级加密标准缓冲器[119:112]*/
#define CC1200_AES_BUFFER13 0x2FF2/*高级加密标准缓冲器[111:104]*/
#define CC1200_AES_BUFFER12 0x2FF3 //高级加密标准缓冲器[103:93]*
#define CC1200_AES_BUFFER11 0x2FF4 /*高级加密标准缓冲器[95:88]*/
#define CC1200_AES_BUFFER10 0x2FF5 /*高级加密标准缓冲器[87:80]*/
#define CC1200_AES_BUFFER9 0x2FF6 //高级加密标准缓冲器[79:72]*
#define CC1200_AES_BUFFER8 0x2FF7 /*高级加密标准缓冲器[71:64]*/
#define CC1200_AES_BUFFER7 0x2FF8 //高级加密标准缓冲器[63:56]*
#define CC1200_AES_BUFFER6 0x2FF9 //高级加密标准缓冲器[55:48]*
#define CC1200_AES_BUFFER5 0x2FFA /*高级加密标准缓冲器[47:40]*/
#define CC1200_AES_BUFFER4 0x2FFB /*高级加密标准缓冲器[39:32]*/
#define CC1200_AES_BUFFER3 0x2FFC /*高级加密标准缓冲器[31:24]*/
#define CC1200_AES_BUFFER2 0x2FFD /*高级加密标准缓冲器[23:16]*/
#define CC1200_AES_BUFFER1 0x2FFE /*高级加密标准缓冲器[15:8]*/
#define CC1200_AES_BUFFER0 0x2FFF /*高级加密标准缓冲器[7:0]*
/*------------------ *
/*------------------ *
/*------------------ *
/*------------------ *
#define SmartRF_RADIO_CC1200
#define SmartRF_setting_IOCFG2 0x06
#define SmartRF_setting_deviation_M 0xD1
#define SmartRF_setting_MODCFG_DEV_E 0x00
#define SmartRF_setting_DCFILT_CFG 0x5D
#define SmartRF_setting_帧 头_CFG0 0x8A
#define SmartRF_setting_IQIC 0xCB
#define SmartRF_setting_CHAN_BW 0xA6
#define SmartRF_setting_MDMCFG1 0x40
#define SmartRF_setting_MDMCFG0 0x05
#define SmartRF_setting_symbol_Rate2 0x3F
#define SmartRF_setting_symbol_rate1 0x75
#define SmartRF_setting_symbol_RATE0 0x10
#define SmartRF_setting_AGC_REF 0x20
#define SmartRF_setting_AGC_CS_THR 0xEC
#define SmartRF_setting_AGC_CFG1 0x51
#define SmartRF_setting_AGC_CFG0 0x87
#define SmartRF_setting_FIFO_CFG 0x00
#define SmartRF_setting_FS_CFG 0x14
#define SmartRF_setting_PKT_CFG2 0x00
#define SmartRF_setting_PKT_CFG0 0x20
#define SmartRF_setting_PKT_LEN 0xFF
#define SmartRF_setting_if_Mix_CFG 0x1C
#define SmartRF_setting_FREQOFF_CFG 0x22
#define SmartRF_setting_MDMCFG2 0x0C
#define SmartRF_setting_FREQ2 0x57
#define SmartRF_setting_if_ADC1 0xEE
#define SmartRF_setting_if_ADC0 0x10
#define SmartRF_setting_FS_DIG1 0x07
#define SmartRF_setting_FS_DIG0 0xAF
#define SmartRF_setting_FS_CAL1 0x40
#define SmartRF_setting_FS_CAL0 0x0E
#define SmartRF_setting_FS_DIVTWO 0x03
#define SmartRF_setting_FS_DSM0 0x33
#define SmartRF_setting_FS_DVC0 0x17
#define SmartRF_setting_FS_PFD 0x00
#define SmartRF_setting_FS_PRE 0x6E
#define SmartRF_setting_FS_REG_DIV_CML 0x1C
#define SmartRF_setting_FS_SPARE 0xAC
#define SmartRF_setting_FS_VCO0 0xB5
#define SmartRF_setting_XOSC5 0x0E
#define SmartRF_setting_XOSC1 0x03