主题中讨论的其他部件:UNIFLAASH, CC3135, CC31XXEMUBOOST, CC3220S, CC3220SF, CC3235S, CC3235SF
您好,
查看uniflifliflif_csr.0目录中的文档,特别是关于通过命令行与映像创建者和csr.exe工具(使用get_csr.bat脚本)自动生成7.2 的文档-是否可以通过CC31XXEMUBOOST平台与CC3135一起使用?
get_csr.bat脚本的部件选项包括:
- CC3220S
- CC3220SF
- CC3235S
- CC3235SF
我对每一款都有一个想法,希望CC3235S在CC3135上仍能正常工作,但当脚本到达需要关闭主板电源然后再打开时,脚本就会掉下来。 我不确定这是否只是要求断开EMUBOOST的USB连接(尽管这也不起作用-脚本在我重新插入之前失败),或者它是否正在寻找可直接连接到CC3135的USB。
这对于能够通过生成,提取和签署CSR自动配置CC3135主板非常有用,签名证书将重新加载。 我在下面附上了Get_CSR输出的尾端。 目前,我只是使用脚本中的默认值,并配置了以下路径:
设置UNIFLEASHPATH="%BATFILEPATH%..\bin"
设置SDKINSTALLPATH=C:\ti\simplelink_cc32xx_SDK_5_10_00_02
远程*****
REM Service Pack名称和路径
设置4.10 3.1 .3.7 0.26 .bin
set sp_path="%SDKINSTALLPATH%/tools/cc32xx_tools/servicepack-cc3x35"(设置SP_PATH="%SDKINSTALLPATH%/tools/cc32xx_tools/servicepack-cc3x35")
REM证书存储列表/签名和路径
设置CERT_LST=certcatalogPlayGround2016.0911万.lst
设置CERT_LST_BIN=certcatalogPlayGround2016.0911万.lst.signed_3235.bin</s>3235.
set CERT_LST_PATH="%SDKINSTALLPATH%/tools/cc32xx_tools/certificate-fally"(设置CERT_LST_PATH="%SDKINSTALLPATH%/tools/cc32xx_tools/certificate-fally
REM证书名称,密钥和路径
设置dummy_cert_name=dummed-root-ca-cert
设置dumm_key_name=dummed-root-ca-cert-key
SET DUMMY_CERT_PATH="%SDKINSTALLPATH%/TOOL/CC32xx_TOOLS/certificate-fally"(设置dummy_CERT_PATH="%SDKINSTALLPATH%/tools/cc32xx_tools/certificate-
Non-encrypted files generated successfully. Finished successfully. INFO:root:COM PORT COM3 INFO:slbootloader.slbootloader:Connecting to device INFO:slbootloader.slbootloader:--- Please power off the device --- Press ENTER to continue INFO:slbootloader.slbootloader:Power off INFO:slbootloader.slbootloader:Set break signal INFO:slbootloader.slbootloader:--- Please power on the device --- INFO:slbootloader.slbootloader:Power on Traceback (most recent call last): File "<string>", line 5266, in <module> File "<string>", line 5262, in main File "<string>", line 5232, in cmdline File "<string>", line 4077, in command_project_program File "<string>", line 2706, in program_image_from_project File "<string>", line 1567, in connect_device File "W:\slbootloader\slbootloader.py", line 409, in connect_with_reset File "W:\slbootloader\slbootloader.py", line 271, in _expect_ack File "W:\slbootloader\slbootloader.py", line 302, in _read_data slbootloader.slbootloader.BootLoaderError: Error: SLImageCreator.exe: BootLoaderError, Timeout reading data SLImageCreator returned -1 sleep 10 reset device ERROR: Failed to connect to XDS110 (-260). Check USB connection to the XDS110. popd pushd c:\ti\uniflash_7.2.0\simplelink\imagecreator\csr\