如题,想请教下,购买的LAUNCHXL-F28377S LaunchPad中内部预置的串口+ADC+LED程序在哪里可以下载?
预置程序实现如下功能:When the LaunchPad is connected via USB, the demo starts with an LED flash sequence. After a few seconds the device switches into an ADC sample mode. Each second the ADC is sampled and the sample data is relayed to you. If the sample is above mid-scale (2048), the red LED will light. However, if the sample is below mid-scale the blue LED will light.