Part Number: TMS320F280039C
Other Parts Discussed in Thread: TIDA-010938, TMDSCNCD280039C
我们根据官网提供的资料自己制作了TIDA-010938的AC/DC部分底板,购买了TMDSCNCD280039C控制卡。测试运行实验6,
//Select the test lab to be used
#define SINV_LAB 6
//Select the modulation scheme here : 1 for HERIC, 2 for Bipolar, 3 for Unipolar
#define stringINV_DCAC_Modulation_Scheme 2
并根据软件说明在DC/DC端加载了50V直流电压。为了防止运行故障,我们没有连接跳线J4/J5/J13/J21和J22,而是将对应的PWM输出接到了逻辑分析仪上。得到波形如下图:

图中第一路信号接J22的S1,第二路信号接J4的S2,第三路信号接J5的S5,第四路信号接J13的S6。运行出来的结果波形如上图。我们感觉这个波形不太对。连接仿真器看了一。发现程序运行到stringINV.h的