This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320LF2407A: Win10系统中,脱离CCS,通过仿真器(如XDS510-USB),对TMS320LF2407A下载程序(out文件)。

Part Number: TMS320LF2407A

以往,使用 安装于XP系统的 CCS3.1开发的,基于TMS320LF2407A的程序。

现在需要对程序进行修改。但是XP系统的电脑使用不方便了。

所以,目前在Win10系统中,采用虚拟机的方案安装了XP系统,并安装了CCS3.1,

可以实现对程序的修改了,并得到了out文件。

但是,在虚拟机的XP系统中,使用仿真器对TMS320LF2407A下载程序,速度相当慢,非常慢,容易出错。

请问:有没有这样的工具软件,在Win10系统,脱离CCS独立运行,并可以使用仿真器(如XDS510)对TMS320LF2407A下载程序(.out文件)。