This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP28035自制板无法烧写,错误501

各位前辈们好:

我设计了一个使用28035的传感器,供电为24v,经过两级标准LM2596-5.0+TPS73033转出3.3v供CPU使用,上电后DSP的3.3引脚电压都为3.29v,1.8引脚电压为1.91v,但在连接仿真器时出现以下报错,且无法烧写,经检查电路连通性没有问题。

Error connecting to the target:
(Error -501 @ 0x0)
The built-in scan-path length measurement failed.
The built-in scan-path reliability tests cannot be
performed without knowledge of the scan-path length.
Try specifying the scan-path lengths in the command-line
options or board configuration file of this utility or debugger.
(Emulation package 5.1.450.0)

目前在尝试从手册上找找原因,我想知道有那些可能的原因会造成这个错误501。