Other Parts Discussed in Thread: AMC1203, AMC1204
TI工程师:
您好!
1、请教在TI推出的 Δ-Σ 调制器如AMC1204,AMC1304等时钟信号都需要外部输入,多占用DSP一个管脚。请问为什么不像AMC1203或者ADI的AD7400A那样,芯片本身提供时钟输出呢?AMC1204,AMC1304这样做有什么好处吗?
2、AMC1204有两种封装,SOIC-8和SOIC-16,功能一样吗?为什么要推出两种封装?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
外部时钟输入应该是为了设计的灵活性,比如更好的同步。
如你有更进一步的AMC1204/1304问题,可以到AMC1204/1304相关板块提问。
从设计的角度来说是为了能实现更好的同步,不管是一个AMC1204还是多个ADC1204,以及为了能让客户提供更高精度的时钟。但实际应用的时候,是否有多大影响要看你的CLK频率,个人认为如果CLK为20MHz,OSR够大的话,是否同步应该都没有问题。