This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

基于28377的SDFM采样



本人看到TI有原创的基于AMC1304的SDFM采样方案,参见附件。本人现在的问题是:

1、基于本方案SDFM的时钟可以达到20MHz么?

2、准备将采样部分放到功率板上对电机输出两相电流进行采样,那么作为主控板上的SDFM和功率板上的AMC1304都需要时钟的情况下,怎么保证时钟信号,尤其是在功率板上达到20MHz时候不受干扰,以及到DSP和AMC1304时的同步问题是否需要考虑?

3、在本方案中时钟信号如何获取比较合适?比如之前本论坛有提出从DSP的EPWM输出管脚给出,那么针对远在功率板上的AMC1304来讲是否合适?如果可行,那么有没有其它的补充方案?比如增加高速磁隔离等.

论坛参考链接:www.deyisupport.com/.../115540.aspx

TI_TMS320F28377X_SDFM_AMC1304.pdf
  • 1. 5MHz~20MHz都可以

    2. 比如采用28377上的pwm获得时钟,分别提供给AMC1304(CLKin)和SDFM(SDCx),由于是一个信号,在传输延迟可以忽略的情况下时钟同步的。功率板侧上是一个采样电阻经过滤波器输入到AMC1304上面,不需要时钟信号;时钟信号在隔离之后的另外外一侧。

    3. 采用pwm获取时钟信号可行的。建议布线的时候从时钟信号输出到两个模块的时钟输入的走线一样长。