This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S芯片的SYSPLL一直无法LOCK



1.板子是我自己画的,可以使用JTAG连接板子,下载程序到RAM里面,偶尔可以下载到FLASH里面

通过step into 一步步走,最终发现程序卡死在SysCtrl.C 里的while(ClkCfgRegs.SYSPLLSTS.bit.LOCKS != 1) 这句话,直接运行之后按下暂停也会卡在这里。

2.怀疑可能是:a.板子没焊好,给锁相环供电的引脚虚焊 b.寄存器没有配置好 

3.可是我用官方的launchpad是可以下载并调试的..//

4.不知道还有什么原因会导致这个问题呢?