This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379 RC复位电路,注意事项有哪些?

使用tms320f29379推荐电路使用TPS3895ADRYT作为复位电路时,主板工作正常,但是由于TPS3895ADRYT封装问题,太难焊接,目前取消TPS3895ADRYT,改用RC电路后,发现设备上电后设备不工作,用镊子短接RC电路的电容,设备可以工作;GPIO72\GPIO84均上拉,目前R=10k 、C=100nf;另外想知道tw(RSL1)复位时间是否为严格的100us;请帮忙分析一下可能的故障原因?谢谢

  • "使用tms320f29379推荐电路使用TPS3895ADRYT作为复位电路时,主板工作正常,但是由于TPS3895ADRYT封装问题,太难焊接,目前取消TPS3895ADRYT,改用RC电路后,发现设备上电后设备不工作,用镊子短接RC电路的电容,设备可以工作;GPIO72\GPIO84均上拉,目前R=10k 、C=100nf;"
    ERIC:
    首先,看一下你的电源上电时序,保证如下的上电要求。另外,你可以试着把上拉电阻改小到5K。
    "The voltage on VDDIO should be greater than VDD or no less than 0.3 V below VDD at all times. VDDIO,
    V
    DD3VFL, VDDOSC, and VDDA should be powered up together and be kept within 0.3 V of each other during
    operation. Before powering the device, no voltage larger than 0.3 V above VDDIO should be applied to any
    digital pin, and no voltage larger than 0.3 V above VDDA should be applied to any analog pin.
    An internal power-on-reset (POR) circuit holds the device in reset and keeps the I/Os in a high-impedance
    state during power up. External supply voltage supervisors (SVS) can be used to monitor the voltage on
    the 3.3-V and 1.2-V rails and drive XRS low should supplies fall outside operational specifications."
  • 谢谢   我先核对一下

  • RC只能实现上电自复位 也就是在上电电容充电瞬间实现低到高的变化
    你可以增大电容值看看 有没有改善
    复位电路比较可靠 主要是确保电源准备好 并且可以延时 持续 复位信号