This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2808 PWM模块中下面的理解

不知道下面这段话是什么意思。求老师们解答。谢谢

The specified condition on the pins is automatically cleared when the ePWM time-base counter reaches zero (TBCTR = 0x0000) if the trip condition is no longer present. The condition on the pins is only cleared when the TBCTR = 0x0000 no matter where in the cycle the CBC flag is cleared.

  • CBC是TZ信号出现以后,基于每个周期切断PWM输出的,如果TZ保护信号撤除掉了,那么下一个PWM周期输出将恢复。

    One Shot是TZ保护信号出现则彻底关断PWM输出,在保护信号撤除以后,需要软件清除掉TZ保护寄存器相应标志后,PWM才会继续输出。

  • 老师,还是有点不明白cycle-by-cycle 和 one-shot trip event 

    我们知道:

    a、The trip-zone signals at pins TZ1 to TZ6 (also collectively referred to as TZn) are active low input signals.When one of these pins goes low, it indicates that a trip event has occurred.

    b、Each TZn input can be individually configured to provide either a cycle-by-cycle or one-shot trip event for a ePWM module. The configuration is determined by the TZSEL[CBCn] and TZSEL[OSHTn] control bits (where n corresponds to the trip pin) respectively.

    c、The specified condition on the pins is automatically cleared when the ePWM time-base counter reaches zero (TBCTR = 0x0000) if the trip event is no longer present. Therefore, in this mode, the trip event is cleared or reset every PWM cycle.

    就是每个TZn引脚可以配置成提供cycle-by-cycle 和 one-shot trip event 

    问题如下:

    1.从提供的资料a和b中,a cycle-by-cycle or one-shot trip event各自产生的条件是什么?除了配置TZSEL[CBCn] and TZSEL[OSHTn]之外,还有TZn引脚输入有什么区别才会产生不同的故障事件?

    我是这样想的:one-shot trip event 就是TZn引脚有一个低电平脉冲就产生一个one-shot trip event(符合产生条件);而Tzn引脚必须一连串周期低电平有效脉冲才会产生?

    2.从提供的资料c中,我们可以知道:如果a cycle-by-cycle trip event不存在,这个不存在的条件是什么?

       当TBCTR = 0x0000时,The specified condition on the pins is automatically cleared.我对这个引脚上“specified condition”不明白,指的是哪个引脚?是TZn引脚吗?是指引脚的什么特定条件?对这个自动清除也不明白,自动清除什么?是清零吗?还是清除引脚产生周期事故的条件?

    在这个模式下,the trip event is cleared or reset every PWM cycle .周期事故事件在每个PWM周期下是怎样被清除或者置位的?

  •  没有区别,引脚拉低就会触发事件,具体触发什么事件由配置决定。不存在的条件是TZ引脚不再拉低,那PWM引脚所处的特定状态将清除(请见TZCTL寄存器说明),

    PWM引脚将回复到原有的工作状态。

    在例程包中有一个epwm_trip_zone例程,您可以跑一下试试。

  • 请问跑epwm_trip_zone例程需要怎样设置Gpio 和初始化?我建立了一个工程把例程载入以后调试不能成功,请高手指点,谢谢。