This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HRPWM在高精度周期模式下,B路输出1clk的抖动



需要波形:两路1.511MHz互补输出,带有50ns死区。

将HRPWM配置成高精度周期模式,高精度死区打开。用EPWMA来做高精度输出,EPWMB通过死区模块产生。

现在问题是EPWMA在频率,占空比上都能达到要求,但是通过EPWMA经过DB模块产生的EPWMB波形有1clk(10ns)的抖动。这是什么原因?感觉高精度死区没启作用一样

芯片:280049C,用的TMDSCNCD280049C开发板,配置如下:

RED,FED的值:10,死区半周期模式已打开

CMPA在周期的一半