Part Number: F28M35H52C
Other Parts Discussed in Thread: CONTROLSUITE
现在我编写的C28核和M3核的程序,在连接仿真器的情况下能够正常运行。但是不连仿真器。重新上电之后M3核的程序能够运行(通过LED灯),C28核的程序没有运行(通过LED观察)。在网上寻找了一些答案但是没有解决。例如通过在M3程序设置#define STANDALONE,启动IPCMtoCBootControlSystem(CBROM_MTOC_BOOTMODE_BOOT_FROM_FLASH);,但是这样M3程序运行到此处程序就好跑飞。
#ifdef _STANDALONE
#ifdef _FLASH
// Send boot command to allow the C28 application to begin execution
IPCMtoCBootControlSystem(CBROM_MTOC_BOOTMODE_BOOT_FROM_FLASH);
#else
// Send boot command to allow the C28 application to begin execution
IPCMtoCBootControlSystem(CBROM_MTOC_BOOTMODE_BOOT_FROM_RAM);
#endif
#endif
检测了硬件boot设置。也设置正确(因为M3能够正常启动,所以boot应该设置的没有问题)
CMD文件,都是采用flash.cmd.
一直没有找到解决的方法还请大神指导。