Other Parts Discussed in Thread: ADC14L040,
有以下应用需要dsp同步采集外部高速ADC,每100ms产生1个脉冲,经过一段时间后采集1ms,然后进行处理,需要采样率达到40M,以下问题哈
1>是否可以使用TMS320F28375S的EMIF总线,同步读取ADC14L040数据,ADC14L040所需要的时钟有EMIF模块产生
2>开始采集有,连续的1ms数据不能间断,使用DMA搬运,EMIF是否支持同步突发访问,即发送一个地址后,不停的搬运数据(不在发送地址信号)
3>是否可以通过ePWM产生一个脉冲,然后定时一段时间(几百微秒左右),除非DMA对外部ADC进行同步读取?
如果TMS320F28375S无法完成上述功能,是否有推荐的dsp可以完成上述功能
万分感谢。