This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSCNCD28388D: SCI通讯问题

Part Number: TMDSCNCD28388D

我采用的28388D controlcard ( version B)上的SCIA与PC串口通讯;配置如下:

Controlcard通过金手指直接插到我做的接口板上,接口板上有基于UT3232芯片的SCI通讯电路(3.3V供电);电脑USB通过一个USB转串口连接到该芯片,该芯片的输出连接至controlcard上的GPIO35, GPIO36,将该两个引脚配置成SCIA_RX, SCIA_TX;接收电脑串口调试器发送来的信号。

controlcard的5V电源来自接口板,金手指上多处的gnd信号也和接口板上的gnd连接。

通过示波器看UT3232芯片输出至controcard的SCIA_RX信号(也就是28388D要接收的信号),发现如下问题:

通过串口调试软件,多次发送同一组数据(一次5个byte) 的情况下,如果不把controlcard插在接口板上,那么每次发送的时候波形基本一致,表明发送数据确实一致的;但是当把controlcard插上之后,同一个地方测试SCIA_RX信号,则每次发送显示的波形非常不一致,如果在28388上运行程序,则接收的时候每次也收到不同的数据,而实际上发送的都是一样的数据。

以上问题感觉是硬件的问题,但始终找不到原因。

做过的尝试有,把controlcard上的3.3V电压引出给接口板上的UT3232芯片供电,现象依旧。

各位能否帮我分析一下可能的原因以及解决方法?