This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28021: 正在开发高频UPS,平时编程的芯片为TMS320F28027但领导让用TMS320F28021,我做了改动后,工程编译通过,但就是JTAG无法连通,但28027就可以 请问是什么问题?

Part Number: TMS320F28021
Other Parts Discussed in Thread: TMS320F28027

板子最初焊接的芯片是28021但程序无法下载故换成28027就可以正常下载,此外28021的代码是在28027的工程的基础上下修改的修改的时候把目标芯片改为28021

修改如下

1.#define DSP28_PLLCR   12改为#define DSP28_PLLCR   8

2.#define CPU_RATE   16.667L   // for a 60MHz CPU clock speed (SYSCLKOUT)改为//#define CPU_RATE   25.000L   // for a 40MHz CPU clock speed  (SYSCLKOUT)

3.#define   DSP28_28027PT   TARGET改为#define   DSP28_28027PT   0

4.#define   DSP28_28021PT   0改为#define   DSP28_28021PT   TARGET

5.并且在CCS中把CMD文件有原来的F28027.cmd更改为F28021.cmd

但CMD做了更改后发现.text 有误 故在CMD做了更改后结果错误

是不是还要更改DSP2802x_Headers_nonBIOS.cmd这个文件?

请问由28027的工程改为28021使用需要做哪些更改?

我用的是代码下载到flash中的工程

谢谢!