在TPS62420DRCR中,1.2V由TPS62420DRCR产生,
TPS62420DRCR产生的1.2V是数字电源,按理说这个1.2V是不是可以直接连接至28388的VDD引脚。
为什么在TPS62420DRCR中,这个1.2V还要经过一个电感变为VDD_1V2连接到VDD引脚呢?
这里的L5是不是可以省掉
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在TPS62420DRCR中,1.2V由TPS62420DRCR产生,
TPS62420DRCR产生的1.2V是数字电源,按理说这个1.2V是不是可以直接连接至28388的VDD引脚。
为什么在TPS62420DRCR中,这个1.2V还要经过一个电感变为VDD_1V2连接到VDD引脚呢?
这里的L5是不是可以省掉
就F28388D来说是不需要这个电感的,手册在只明确了需要去耦电容:
1.2-V Digital Logic Power Pins. TI recommends placing a decoupling capacitor near each VDD pin with a minimum total capacitance of approximately 20 µF. The exact value of the decoupling capacitance should be determined by your system voltage regulation solution. A single 56Ω resistor (10% tolerance) should be placed between between VDD and VSS. This resistor provides a load to consume an internal VDD3VFL to VDD current source and avoid VDD voltage rising during low power device conditions.
不知道是否跟TPS62420DRCR有关,你可以去咨询一下电源芯片的工程师。
另外很奇怪这里的电感值是标的是220ohm
您好 刚才想了一下 这里的两个电容加一个磁珠 是构成了π型滤波器
220ohm是磁珠的特征阻抗
因为要求VDD的退耦合电容大约在20uF左右 所以这里的电容用了2个10uF