Other Parts Discussed in Thread: SM73201
我想在28033上外扩一个精度更高的AD芯片SM73201,但是不知道该怎么设置处理器。
(1) 是通过SPI模块和DA芯片通讯吗?
(2) 那么只要设置CLK的时钟就可以了么?
(3) 如果我已经确定了最低的采样频率,比如200K,那么CLK这个时钟的频率该怎么计算?
问题有点多,本人菜鸟,谢谢大家!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SM73201
我想在28033上外扩一个精度更高的AD芯片SM73201,但是不知道该怎么设置处理器。
(1) 是通过SPI模块和DA芯片通讯吗?
(2) 那么只要设置CLK的时钟就可以了么?
(3) 如果我已经确定了最低的采样频率,比如200K,那么CLK这个时钟的频率该怎么计算?
问题有点多,本人菜鸟,谢谢大家!
Jason Wang2 ,谢谢!
其实我更关注后面两个问题~能不能为我详细解答下呢?谢谢!
The external SCLK controls data transfer and serves as the conversion clock. The duty cycle of SCLK is essentially unimportant, provided the minimum clock high and low times are met. The minimum SCLK frequency is set by internal capacitor leakage.
外部的时钟SCLK控制AD芯片的转换率,并作为转换时钟。
一般来讲,换速率为200KHZ,时钟频率Fclk=16*Fsample,时钟频率为3.2Mhz。你不妨试试给一个3.2M的CLK,看看对不对。